public static class PostGraphBuilder.GeometryValue extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AVERAGE |
static int |
_INTEGRAL |
static int |
_MAXIMUM |
static int |
_MINIMUM |
static int |
_SUM |
static int |
_WEIGHTED_AVERAGE |
static PostGraphBuilder.GeometryValue |
AVERAGE |
static PostGraphBuilder.GeometryValue |
INTEGRAL |
static PostGraphBuilder.GeometryValue |
MAXIMUM |
static PostGraphBuilder.GeometryValue |
MINIMUM |
static PostGraphBuilder.GeometryValue |
SUM |
static PostGraphBuilder.GeometryValue |
WEIGHTED_AVERAGE |
Modifier and Type | Method and Description |
---|---|
static PostGraphBuilder.GeometryValue |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PostGraphBuilder.GeometryValue |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PostGraphBuilder.GeometryValue[] |
values()
Returns an array that contains the values for this enum.
|
public static final PostGraphBuilder.GeometryValue AVERAGE
public static final PostGraphBuilder.GeometryValue MINIMUM
public static final PostGraphBuilder.GeometryValue MAXIMUM
public static final PostGraphBuilder.GeometryValue SUM
public static final PostGraphBuilder.GeometryValue WEIGHTED_AVERAGE
public static final PostGraphBuilder.GeometryValue INTEGRAL
public static final int _AVERAGE
public static final int _MINIMUM
public static final int _MAXIMUM
public static final int _SUM
public static final int _WEIGHTED_AVERAGE
public static final int _INTEGRAL
public static PostGraphBuilder.GeometryValue valueOf(int value)
public static PostGraphBuilder.GeometryValue valueOf(String name)
public static PostGraphBuilder.GeometryValue[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.