public interface PostGraphAcrossIterationsBuilder extends PostGraphBuilder
PostGraphAcrossIterationsBuilder
Modifier and Type | Interface and Description |
---|---|
static class |
PostGraphAcrossIterationsBuilder.CombinationMethod
Defines the methods that can be used to combine multiple values into a single value
|
static class |
PostGraphAcrossIterationsBuilder.IterationLabelingOption
Defines the Iteration labeling options
|
PostGraphBuilder.DataErrorHandling, PostGraphBuilder.EdgeIntegralOption, PostGraphBuilder.EntityType, PostGraphBuilder.EvalutionErrors, PostGraphBuilder.FaceIntegralOption, PostGraphBuilder.GeometryValue, PostGraphBuilder.IncompatibleResult, PostGraphBuilder.NodalCombination
Modifier and Type | Method and Description |
---|---|
boolean |
combineAcrossEntities()
Returns the combine across entities method to be used if
combineAcrossEntities() and setCombineAcrossEntities(boolean) is True
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX9.0.0 |
PostGraphAcrossIterationsBuilder.CombinationMethod |
combineValueFromEntitiesOption()
Returns the set combine across entities option type
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
int |
iterationStepSpacing()
Returns the step spacing to be used between the start and end iteration.
|
PostGraphAcrossIterationsBuilder.IterationLabelingOption |
iterationValueOption()
Returns the select iteration type to be set as x axis
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setCombineAcrossEntities(boolean combineAcrossEntities)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setCombineValueFromEntitiesOption(PostGraphAcrossIterationsBuilder.CombinationMethod combineOption)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setEndIteration(BaseIteration iteration)
Set end iteration
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setIterationStepSpacing(int iterationStepSpacing)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setIterationValueOption(PostGraphAcrossIterationsBuilder.IterationLabelingOption iterationValue)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setStartIteration(BaseIteration iteration)
Set start iteration
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
complexGraphTypes, createFieldOption, edgeIntegralOptionValue, evalutionErrorsOption, faceIntegralOptionValue, geometryCombinationValue, getFieldTable, graphTitle, incompatibleResultOption, nodalCombinationValue, noDataOption, saveAfuOption, selectedEntityType, setComplexGraphTypes, setCreateFieldOption, setEdgeIntegralOptionValue, setEntityIds, setEntityObjects, setEvalutionErrorsOption, setFaceIntegralOptionValue, setFreePoints, setGeometryCombinationValue, setGraphTitle, setIncompatibleResultOption, setNodalCombinationValue, setNoDataOption, setSaveAfuOption, setSelectedEntityType, setUserData, userData
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
PostGraphAcrossIterationsBuilder.IterationLabelingOption iterationValueOption() throws NXException, RemoteException
NXException
RemoteException
void setIterationValueOption(PostGraphAcrossIterationsBuilder.IterationLabelingOption iterationValue) throws NXException, RemoteException
iterationValue
- NXException
RemoteException
void setStartIteration(BaseIteration iteration) throws NXException, RemoteException
iteration
- NXException
RemoteException
void setEndIteration(BaseIteration iteration) throws NXException, RemoteException
iteration
- NXException
RemoteException
int iterationStepSpacing() throws NXException, RemoteException
NXException
RemoteException
void setIterationStepSpacing(int iterationStepSpacing) throws NXException, RemoteException
iterationStepSpacing
- NXException
RemoteException
boolean combineAcrossEntities() throws NXException, RemoteException
combineAcrossEntities()
and setCombineAcrossEntities(boolean)
is True
NXException
RemoteException
void setCombineAcrossEntities(boolean combineAcrossEntities) throws NXException, RemoteException
combineAcrossEntities
- NXException
RemoteException
PostGraphAcrossIterationsBuilder.CombinationMethod combineValueFromEntitiesOption() throws NXException, RemoteException
NXException
RemoteException
void setCombineValueFromEntitiesOption(PostGraphAcrossIterationsBuilder.CombinationMethod combineOption) throws NXException, RemoteException
combineOption
- NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.