SimDebugBuilder Class¶
-
class
NXOpen.SIM.
SimDebugBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.SIM.SimDebugBuilder
To create a new instance of this class, use
NXOpen.SIM.KinematicConfigurator.CreateSimDebugBuilder()
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Driver | Returns or sets the driver |
Dump | Returns or sets the dump |
DumpOutput | Returns or sets the dump output |
DumpToFileName | Returns or sets the output filename |
KinematicModel | Returns or sets the kinematic model |
PrintoutTags | Returns or sets the printout tags type |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetTrace | Gets the trace @return The state |
GetUiSetting | Gets the debug setting @return The state |
SetTrace | Sets the trace |
SetUiSetting | Sets the debug setting |
ShowKinematicModelState | Show the kinematic model state |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SimDebugBuilderDriverType Enumeration | Represents the driver type |
SimDebugBuilderDumpType Enumeration | Represents the dump type |
SimDebugBuilderKinematicModelType Enumeration | Represents the kinematic model type |
SimDebugBuilderOutputType Enumeration | The output type |
SimDebugBuilderPrintoutTagsOrPointersType Enumeration | Represents the printout tags or pointers type |
SimDebugBuilderTraceType Enumeration | Represents the trace type |
SimDebugBuilderUiType Enumeration | Represents the ui type |
Property Detail¶
Driver¶
-
SimDebugBuilder.
Driver
¶ Returns or sets the driver
-------------------------------------
Getter Method
Signature
Driver()
Returns: Return type: NXOpen.SIM.SimDebugBuilderDriverType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Driver(type)
Parameters: type ( NXOpen.SIM.SimDebugBuilderDriverType
) – The driver typeNew in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
Dump¶
-
SimDebugBuilder.
Dump
¶ Returns or sets the dump
-------------------------------------
Getter Method
Signature
Dump()
Returns: The dump type Return type: NXOpen.SIM.SimDebugBuilderDumpType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Dump(type)
Parameters: type ( NXOpen.SIM.SimDebugBuilderDumpType
) – The dump typeNew in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
DumpOutput¶
-
SimDebugBuilder.
DumpOutput
¶ Returns or sets the dump output
-------------------------------------
Getter Method
Signature
DumpOutput()
Returns: The dump output type Return type: NXOpen.SIM.SimDebugBuilderOutputType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DumpOutput(type)
Parameters: type ( NXOpen.SIM.SimDebugBuilderOutputType
) – The dump output typeNew in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
DumpToFileName¶
-
SimDebugBuilder.
DumpToFileName
¶ Returns or sets the output filename
-------------------------------------
Getter Method
Signature
DumpToFileName()
Returns: The output name Return type: str New in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
-------------------------------------
Setter Method
Signature
DumpToFileName(name)
Parameters: name (str) – the output new name New in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
KinematicModel¶
-
SimDebugBuilder.
KinematicModel
¶ Returns or sets the kinematic model
-------------------------------------
Getter Method
Signature
KinematicModel()
Returns: Return type: NXOpen.SIM.SimDebugBuilderKinematicModelType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KinematicModel(type)
Parameters: type ( NXOpen.SIM.SimDebugBuilderKinematicModelType
) – The kinematic model typeNew in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
PrintoutTags¶
-
SimDebugBuilder.
PrintoutTags
¶ Returns or sets the printout tags type
-------------------------------------
Getter Method
Signature
PrintoutTags()
Returns: The printout tags type Return type: NXOpen.SIM.SimDebugBuilderPrintoutTagsOrPointersType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PrintoutTags(type)
Parameters: type ( NXOpen.SIM.SimDebugBuilderPrintoutTagsOrPointersType
) – The printout tags typeNew in version NX8.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
Method Detail¶
GetTrace¶
-
SimDebugBuilder.
GetTrace
¶ Gets the trace
Signature
GetTrace(type)
Parameters: type ( NXOpen.SIM.SimDebugBuilderTraceType
) – The trace typeReturns: The state Return type: bool New in version NX8.0.0.
License requirements: None.
GetUiSetting¶
-
SimDebugBuilder.
GetUiSetting
¶ Gets the debug setting
Signature
GetUiSetting(type)
Parameters: type ( NXOpen.SIM.SimDebugBuilderUiType
) – The ui typeReturns: The state Return type: bool New in version NX8.0.0.
License requirements: None.
SetTrace¶
-
SimDebugBuilder.
SetTrace
¶ Sets the trace
Signature
SetTrace(type, state)
Parameters: - type (
NXOpen.SIM.SimDebugBuilderTraceType
) – The trace type - state (bool) – The state
New in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
- type (
SetUiSetting¶
-
SimDebugBuilder.
SetUiSetting
¶ Sets the debug setting
Signature
SetUiSetting(type, state)
Parameters: - type (
NXOpen.SIM.SimDebugBuilderUiType
) – The ui type - state (bool) – The state
New in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
- type (
ShowKinematicModelState¶
-
SimDebugBuilder.
ShowKinematicModelState
¶ Show the kinematic model state
Signature
ShowKinematicModelState()
New in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
Validate¶
-
SimDebugBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.