SimDebugBuilderDumpType Enumeration¶
NXOpen.SIM.SimDebugBuilder.DumpType is an alias for NXOpen.SIM.SimDebugBuilderDumpType
-
class
NXOpen.SIM.
SimDebugBuilderDumpType
¶ Bases:
object
Represents the dump type
Enum Members
Enum Member Enum Member Description NotSet Dump NothingKinematicModel Dump Kinematic ModelHighlighting Dump HighlightingIpw Dump IPWCollision Dump CollisionOutputBuffer Dump Output BufferTime Dump TimeDetails Dump DetailsSynchronizeUi Dump Synchronize UISynchronizeManagerXtp Dump SynchronizeManagerXtpEngineParams Dump Engine ParamsMomVariables Dump Mom VariablesDebugUi Dump Debug UISimulationSettings Dump Simulation SettingsSimManager Dump SimManagerPathEvents Dump Path Events-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-