SimDebugBuilderTraceType Enumeration¶
NXOpen.SIM.SimDebugBuilder.TraceType is an alias for NXOpen.SIM.SimDebugBuilderTraceType
-
class
NXOpen.SIM.
SimDebugBuilderTraceType
¶ Bases:
object
Represents the trace type
Enum Members
Enum Member Enum Member Description ButtonDown Trace Button DownVcr Trace VcrIpw Trace IpwPerformance Trace PerformanceCollision Trace CollisionGouge Trace GougeHighlighting Trace HighlightingDetails Trace DetailsPositionalIsv Trace Positional IsvSpinningNonSpinning Trace Spinning NonspinningKinematicModel Trace Kinematic ModelEvent Trace EventLineServer Trace Line ServerSync Trace SyncDctkSettings Trace Dctk SettingsDctkMovements Trace Dctk MovementsDctkDisplay Trace Dctk DisplayDctkCollision Trace Dctk CollisionToolPathPicking Trace ToolPath Picking-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-