SimDebugBuilderUiType Enumeration¶
NXOpen.SIM.SimDebugBuilder.UiType is an alias for NXOpen.SIM.SimDebugBuilderUiType
-
class
NXOpen.SIM.
SimDebugBuilderUiType
¶ Bases:
object
Represents the ui type
Enum Members
Enum Member Enum Member Description DisplayMomEvent Display Mom EventShowPartAndTipJunctions Show Part And Tip JunctionGenerateSpinningTools Generate Spinning ToolsUseHybridGougeChecker Use Hybrid Gouge CheckerUseMtbOldDialogs Use MTB Old DialogsUseFastTicker Use Fast TickerPrintOutTraceSerialNumbers Print Out Trace Serial NumbersPerformanceDisplayDetail Performance Display DetailPerformanceDisplayTime Performance Display TimePerformanceIndentTime Performance Indent TimePerformanceDisplayData Performance Display DataDctkWriteCollisionPairs Write Collision Pairs-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-