ViewVisualizationVisual Class¶
-
class
NXOpen.Preferences.
ViewVisualizationVisual
¶ Bases:
object
Represents the set of View related Visualization visual preferences
To obtain an instance of this class, refer to
NXOpen.View
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
DisplayAppearance | Returns or sets the rendering style and the edge display options of the view. |
HiddenEdgeStyle | Returns or sets the hidden edge display style for shaded faces in the view. |
ShadedEdgeColor | Returns or sets the edge color for shaded faces in the view. |
ShadedEdgeStyle | Returns or sets the edge display style for shaded faces in the view. |
ShininessData | Returns or sets the shininess value. |
SurfaceDisplay | Returns or sets the rendering style and the edge display options of the view. |
TrueSurfaceDisplay | Returns or sets the true surface display parameters. |
TwoSidedLight | Returns or sets the two sided light flag. |
Methods¶
Enumerations¶
ViewVisualizationVisualDisplayModeType Enumeration | Describes the available display mode types. |
ViewVisualizationVisualHiddenEdgeStyleType Enumeration | Describes how hidden edges are displayed for shaded faces in the view. |
ViewVisualizationVisualHiddenEdges Enumeration | Describes the appearance of hidden edges displayed in the view. |
ViewVisualizationVisualHiddenEdgesType Enumeration | Describes the available hidden edges types. |
ViewVisualizationVisualRenderingStyle Enumeration | Describes the rendering style for geometry displayed in the view. |
ViewVisualizationVisualShadedEdgeStyleType Enumeration | Describes how edges are displayed for shaded faces in the view. |
ViewVisualizationVisualSmoothEdgeFont Enumeration | Describes all possible font selection for visible smooth edges |
ViewVisualizationVisualSmoothEdgeWidth Enumeration | Describes all possible width selection for visible smooth edges |
Structs¶
ViewVisualizationVisualDisplayAppearanceOptions_Struct Struct | Describes the rendering style and the appearance of edges and silhouettes in the view. |
ViewVisualizationVisualSurfaceDisplayOptions_Struct Struct | Describes the appearance of edges and silhouettes in the view. |
ViewVisualizationVisualTrueSurfaceDisplayPref_Struct Struct | Represents the various surface display parameters. |
Property Detail¶
DisplayAppearance¶
-
ViewVisualizationVisual.
DisplayAppearance
¶ Returns or sets the rendering style and the edge display options of the view.
-------------------------------------
Getter Method
Signature
DisplayAppearance()
Returns: Return type: NXOpen.Preferences.ViewVisualizationVisualDisplayAppearanceOptions_Struct
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplayAppearance(displayAppearanceOptions)
Parameters: displayAppearanceOptions ( NXOpen.Preferences.ViewVisualizationVisualDisplayAppearanceOptions_Struct
) –New in version NX8.5.0.
License requirements: None.
ShadedEdgeColor¶
-
ViewVisualizationVisual.
ShadedEdgeColor
¶ Returns or sets the edge color for shaded faces in the view.
-------------------------------------
Getter Method
Signature
ShadedEdgeColor()
Returns: Return type: int New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShadedEdgeColor(shadedEdgeColor)
Parameters: shadedEdgeColor (int) – New in version NX4.0.0.
License requirements: None.
ShadedEdgeStyle¶
-
ViewVisualizationVisual.
ShadedEdgeStyle
¶ Returns or sets the edge display style for shaded faces in the view.
-------------------------------------
Getter Method
Signature
ShadedEdgeStyle()
Returns: Return type: NXOpen.Preferences.ViewVisualizationVisualShadedEdgeStyleType
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShadedEdgeStyle(shadedEdgeStyle)
Parameters: shadedEdgeStyle ( NXOpen.Preferences.ViewVisualizationVisualShadedEdgeStyleType
) –New in version NX4.0.0.
License requirements: None.
ShininessData¶
-
ViewVisualizationVisual.
ShininessData
¶ Returns or sets the shininess value.
Specifies the intensity of the graphics driver addition of highlights to shaded surfaces, making them appear shiny. The value 0.0 adds no shininess, and 1.0 adds the maximum amount of shininess.
-------------------------------------
Getter Method
Signature
ShininessData()
Returns: Return type: float New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShininessData(shininessData)
Parameters: shininessData (float) – New in version NX3.0.0.
License requirements: None.
SurfaceDisplay¶
-
ViewVisualizationVisual.
SurfaceDisplay
¶ Returns or sets the rendering style and the edge display options of the view.
-------------------------------------
Getter Method
Signature
SurfaceDisplay()
Returns: Return type: NXOpen.Preferences.ViewVisualizationVisualSurfaceDisplayOptions_Struct
New in version NX4.0.0.
Deprecated since version NX8.5.0: Use
NXOpen.Preferences.ViewVisualizationVisual.DisplayAppearance()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
SurfaceDisplay(surfaceDisplay)
Parameters: surfaceDisplay ( NXOpen.Preferences.ViewVisualizationVisualSurfaceDisplayOptions_Struct
) –New in version NX4.0.0.
Deprecated since version NX8.5.0: Use
NXOpen.Preferences.ViewVisualizationVisual.DisplayAppearance()
instead.License requirements: None.
TrueSurfaceDisplay¶
-
ViewVisualizationVisual.
TrueSurfaceDisplay
¶ Returns or sets the true surface display parameters.
-------------------------------------
Getter Method
Signature
TrueSurfaceDisplay()
Returns: Return type: NXOpen.Preferences.ViewVisualizationVisualTrueSurfaceDisplayPref_Struct
New in version NX3.0.0.
Deprecated since version NX4.0.0: Use
NXOpen.Preferences.ViewVisualizationVisual.DisplayAppearance()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
TrueSurfaceDisplay(trueSurfaceDisplay)
Parameters: trueSurfaceDisplay ( NXOpen.Preferences.ViewVisualizationVisualTrueSurfaceDisplayPref_Struct
) –New in version NX3.0.0.
Deprecated since version NX4.0.0: Use
NXOpen.Preferences.ViewVisualizationVisual.DisplayAppearance()
instead.License requirements: None.
TwoSidedLight¶
-
ViewVisualizationVisual.
TwoSidedLight
¶ Returns or sets the two sided light flag.
Specifies whether lighting should be applied to both the front and backsides of faces. If it is true, then lighting from a light source is applied to the front or the back face, depending on which side is exposed to the light source. If this is false, then lighting is not applied to the back of a face even if the back is exposed to the light source.
-------------------------------------
Getter Method
Signature
TwoSidedLight()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TwoSidedLight(twoSidedLight)
Parameters: twoSidedLight (bool) – New in version NX3.0.0.
License requirements: None.