ViewVisualizationVisualDisplayModeType Enumeration¶
NXOpen.Preferences.ViewVisualizationVisual.DisplayModeType is an alias for NXOpen.Preferences.ViewVisualizationVisualDisplayModeType
-
class
NXOpen.Preferences.
ViewVisualizationVisualDisplayModeType
¶ Bases:
object
Describes the available display mode types.
Specifies shading parameters for the selected view. .. deprecated:: NX4.0.0
Enum Members
rendered according to material and texture characteristics assigned to them “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-