ViewVisualizationVisualSmoothEdgeWidth Enumeration

NXOpen.Preferences.ViewVisualizationVisual.SmoothEdgeWidth is an alias for NXOpen.Preferences.ViewVisualizationVisualSmoothEdgeWidth

class NXOpen.Preferences.ViewVisualizationVisualSmoothEdgeWidth

Bases: object

Describes all possible width selection for visible smooth edges

Enum Members

Enum Member Enum Member Description
Original  
Thin  
Normal  
Thick  
One  
Two  
Three  
Four  
Five  
Six  
Seven  
Eight  
Nine  
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.