ViewVisualizationVisualHiddenEdgesType Enumeration

NXOpen.Preferences.ViewVisualizationVisual.HiddenEdgesType is an alias for NXOpen.Preferences.ViewVisualizationVisualHiddenEdgesType

class NXOpen.Preferences.ViewVisualizationVisualHiddenEdgesType

Bases: object

Describes the available hidden edges types.

Determines how hidden edges are displayed in the selected view. .. deprecated:: NX4.0.0

Enum Members

as solid lines “
“Invisible”, ” grid line display of all existing and subsequently

created solid bodies in the selected view, except that portions of geometry and text that appear behind solid bodies are erased “

“Dashed”, ” grid line display of all existing and subsequently

created solid bodies in the selected view, except that all portions of the geometry and text that appear behind solid bodies are displayed as dashed lines “

“GrayThin”, ” All hidden edges in the color gray, with solid font
and thin width. “
“HiddenSurface”, ” Faceted display of all existing and subsequently

created bodies in the selected view “

ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.