JointBuilder Class¶
-
class
NXOpen.Motion.
JointBuilder
¶ Bases:
NXOpen.Motion.MotionBuilder
This builder class is used to create or edit
NXOpen.Motion.Joint
objects.To create a new instance of this class, use
NXOpen.Motion.JointCollection.CreateJointBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
DisplayScale | Returns or sets the icon display scale |
GroupName | Returns or sets the group name |
GroupType | Returns or sets the group type |
JointDefine | Returns the joint define |
JointFriction | Returns the joint friction |
JointMultiDrivers | Returns the driver multi operations : DriverMultiOperations Block |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
JointDefine¶
-
JointBuilder.
JointDefine
¶ Returns the joint define
-------------------------------------
Getter Method
Signature
JointDefine()
Returns: The Joint define Return type: NXOpen.Motion.JointDefine
New in version NX5.0.0.
License requirements: mechanisms (“MECHANISMS”)
JointFriction¶
-
JointBuilder.
JointFriction
¶ Returns the joint friction
-------------------------------------
Getter Method
Signature
JointFriction()
Returns: The Joint friction Return type: NXOpen.Motion.JointFriction
New in version NX5.0.0.
License requirements: mechanisms (“MECHANISMS”)
JointMultiDrivers¶
-
JointBuilder.
JointMultiDrivers
¶ Returns the driver multi operations : DriverMultiOperations Block
-------------------------------------
Getter Method
Signature
JointMultiDrivers()
Returns: The driver multi operations Return type: NXOpen.Motion.DriverMultiOperations
New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
Method Detail¶
Validate¶
-
JointBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.