JointFriction Class¶
-
class
NXOpen.Motion.
JointFriction
¶ Bases:
NXOpen.TaggedObject
Represents a joint friction object
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AdamsFriction | Returns the joint adams friction |
Enable | Returns or sets the option of included |
LmsFriction | Returns the joint lms friction |
RecurDynFriction | Returns the joint recurdyn friction |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
AdamsFriction¶
-
JointFriction.
AdamsFriction
¶ Returns the joint adams friction
-------------------------------------
Getter Method
Signature
AdamsFriction()
Returns: The adams friction Return type: NXOpen.Motion.JointFrictionAdams
New in version NX5.0.0.
License requirements: mechanisms (“MECHANISMS”)
Enable¶
-
JointFriction.
Enable
¶ Returns or sets the option of included
-------------------------------------
Getter Method
Signature
Enable()
Returns: Return type: bool New in version NX5.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
Enable(enable)
Parameters: enable (bool) – New in version NX5.0.0.
License requirements: mechanisms (“MECHANISMS”)
LmsFriction¶
-
JointFriction.
LmsFriction
¶ Returns the joint lms friction
-------------------------------------
Getter Method
Signature
LmsFriction()
Returns: The lms friction Return type: NXOpen.Motion.JointFrictionLms
New in version NX10.0.0.
License requirements: mechanisms (“MECHANISMS”)
RecurDynFriction¶
-
JointFriction.
RecurDynFriction
¶ Returns the joint recurdyn friction
-------------------------------------
Getter Method
Signature
RecurDynFriction()
Returns: The recurdyn friction Return type: NXOpen.Motion.JointFrictionRecurDyn
New in version NX5.0.0.
License requirements: mechanisms (“MECHANISMS”)