DriverMultiOperations Class¶
-
class
NXOpen.Motion.
DriverMultiOperations
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.Motion.DriverMultiOperations
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
MotionEulerAngle1 | Returns the motion motion euler angle1, it is for revolute joint and cylindrical joint |
MotionPointOnCurve | Returns the motion point on curve, it is for point on curve constraint |
MotionTranslationZ | Returns the motion translation z, it is for slider joint and cylindrical joint |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
MotionEulerAngle1¶
-
DriverMultiOperations.
MotionEulerAngle1
¶ Returns the motion motion euler angle1, it is for revolute joint and cylindrical joint
-------------------------------------
Getter Method
Signature
MotionEulerAngle1()
Returns: Return type: NXOpen.Motion.DriverOperation
New in version NX6.0.0.
License requirements: None.
MotionPointOnCurve¶
-
DriverMultiOperations.
MotionPointOnCurve
¶ Returns the motion point on curve, it is for point on curve constraint
-------------------------------------
Getter Method
Signature
MotionPointOnCurve()
Returns: Return type: NXOpen.Motion.DriverOperation
New in version NX6.0.1.
License requirements: None.
MotionTranslationZ¶
-
DriverMultiOperations.
MotionTranslationZ
¶ Returns the motion translation z, it is for slider joint and cylindrical joint
-------------------------------------
Getter Method
Signature
MotionTranslationZ()
Returns: Return type: NXOpen.Motion.DriverOperation
New in version NX6.0.0.
License requirements: None.