JointCollection Class¶
-
class
NXOpen.Motion.
JointCollection
¶ Bases:
object
Represents a collection of motion joints
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
CreateJointBuilder | Return NXOpen.Motion.JointBuilder object @return JointBuilder object |
FindObject | Finds the NXOpen.Motion.Joint with the given name. |
Method Detail¶
CreateJointBuilder¶
-
JointCollection.
CreateJointBuilder
¶ Return
NXOpen.Motion.JointBuilder
objectSignature
CreateJointBuilder(joint)
Parameters: joint ( NXOpen.Motion.Joint
) –NXOpen.Motion.JointBuilder
to be edited, if None then create a new oneReturns: JointBuilder object Return type: NXOpen.Motion.JointBuilder
New in version NX5.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
JointCollection.
FindObject
¶ Finds the
NXOpen.Motion.Joint
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – Returns: Return type: NXOpen.Motion.Joint
New in version NX5.0.0.
License requirements: mechanisms (“MECHANISMS”)