TransformCageData Class¶
-
class
NXOpen.Features.Subdivision.
TransformCageData
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Features.Subdivision.TransformCageData
builder.To create a new instance of this class, use
NXOpen.Features.Subdivision.SubdivisionBodyCollection.CreateTransformCageData()
Default values.
Property Value CanRelocateToolToSelection true CanReorientToolToSelection true New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
CageManipulator | Returns the cage manipulation data. |
CanMoveToolOnly | Returns or sets the flag indicating if transformer tool can be moved without transforming the selected cage topology. |
CanRelocateToolToSelection | Returns or sets the flag indicating if transformer tool can be relocated based on cage topology selection. |
CanReorientToolToSelection | Returns or sets the flag indicating if transformer tool can be reoriented based on cage topology selection. |
FallOffFactor | Returns or sets the falloff factor. |
FallOffMethod | Returns or sets the falloff method. |
FallOffObjects | Returns the falloff objects. |
MovementMethod | Returns or sets the movement method. |
MovementPlane | Returns or sets the movement plane. |
MovementVector | Returns or sets the movement vector. |
ScalingMethod | Returns or sets the scaling method. |
Tag | Returns the Tag for this object. |
TransformationMethod | Returns or sets the transformation method. |
WCSOption | Returns or sets the WCS option. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ResetFallOffToLinear | Resets the falloff scale to linear. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
TransformCageDataFallOffMethodType Enumeration | Falloff method types |
TransformCageDataMovementMethodType Enumeration | Movement types |
TransformCageDataScalingMethodType Enumeration | Scaling method |
TransformCageDataTransformationMethodType Enumeration | Transformation method types |
TransformCageDataWCSOptionType Enumeration | WCS principal axis or plane types |
Property Detail¶
CageManipulator¶
-
TransformCageData.
CageManipulator
¶ Returns the cage manipulation data.
-------------------------------------
Getter Method
Signature
CageManipulator()
Returns: Return type: NXOpen.Features.Subdivision.CageManipulatorData
New in version NX9.0.0.
License requirements: None.
CanMoveToolOnly¶
-
TransformCageData.
CanMoveToolOnly
¶ Returns or sets the flag indicating if transformer tool can be moved without transforming the selected cage topology.
-------------------------------------
Getter Method
Signature
CanMoveToolOnly()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CanMoveToolOnly(canMove)
Parameters: canMove (bool) – New in version NX9.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
CanRelocateToolToSelection¶
-
TransformCageData.
CanRelocateToolToSelection
¶ Returns or sets the flag indicating if transformer tool can be relocated based on cage topology selection.
-------------------------------------
Getter Method
Signature
CanRelocateToolToSelection()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CanRelocateToolToSelection(canRelocate)
Parameters: canRelocate (bool) – New in version NX9.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
CanReorientToolToSelection¶
-
TransformCageData.
CanReorientToolToSelection
¶ Returns or sets the flag indicating if transformer tool can be reoriented based on cage topology selection.
-------------------------------------
Getter Method
Signature
CanReorientToolToSelection()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CanReorientToolToSelection(canReorient)
Parameters: canReorient (bool) – New in version NX9.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
FallOffFactor¶
-
TransformCageData.
FallOffFactor
¶ Returns or sets the falloff factor.
-------------------------------------
Getter Method
Signature
FallOffFactor()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FallOffFactor(factor)
Parameters: factor (float) – New in version NX10.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
FallOffMethod¶
-
TransformCageData.
FallOffMethod
¶ Returns or sets the falloff method.
-------------------------------------
Getter Method
Signature
FallOffMethod()
Returns: Return type: NXOpen.Features.Subdivision.TransformCageDataFallOffMethodType
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FallOffMethod(fallOffMethod)
Parameters: fallOffMethod ( NXOpen.Features.Subdivision.TransformCageDataFallOffMethodType
) –New in version NX10.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
FallOffObjects¶
-
TransformCageData.
FallOffObjects
¶ Returns the falloff objects.
-------------------------------------
Getter Method
Signature
FallOffObjects()
Returns: Return type: NXOpen.Features.Subdivision.SelectCageObjectData
New in version NX10.0.0.
License requirements: None.
MovementMethod¶
-
TransformCageData.
MovementMethod
¶ Returns or sets the movement method.
-------------------------------------
Getter Method
Signature
MovementMethod()
Returns: Return type: NXOpen.Features.Subdivision.TransformCageDataMovementMethodType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MovementMethod(movementMethod)
Parameters: movementMethod ( NXOpen.Features.Subdivision.TransformCageDataMovementMethodType
) –New in version NX9.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
MovementPlane¶
-
TransformCageData.
MovementPlane
¶ Returns or sets the movement plane.
-------------------------------------
Getter Method
Signature
MovementPlane()
Returns: Return type: NXOpen.Plane
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MovementPlane(movementPlane)
Parameters: movementPlane ( NXOpen.Plane
) –New in version NX9.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
MovementVector¶
-
TransformCageData.
MovementVector
¶ Returns or sets the movement vector.
-------------------------------------
Getter Method
Signature
MovementVector()
Returns: Return type: NXOpen.Direction
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MovementVector(movementVector)
Parameters: movementVector ( NXOpen.Direction
) –New in version NX9.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
ScalingMethod¶
-
TransformCageData.
ScalingMethod
¶ Returns or sets the scaling method.
-------------------------------------
Getter Method
Signature
ScalingMethod()
Returns: Return type: NXOpen.Features.Subdivision.TransformCageDataScalingMethodType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScalingMethod(scalingMethod)
Parameters: scalingMethod ( NXOpen.Features.Subdivision.TransformCageDataScalingMethodType
) –New in version NX9.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
TransformationMethod¶
-
TransformCageData.
TransformationMethod
¶ Returns or sets the transformation method.
-------------------------------------
Getter Method
Signature
TransformationMethod()
Returns: Return type: NXOpen.Features.Subdivision.TransformCageDataTransformationMethodType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TransformationMethod(method)
Parameters: method ( NXOpen.Features.Subdivision.TransformCageDataTransformationMethodType
) –New in version NX9.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
WCSOption¶
-
TransformCageData.
WCSOption
¶ Returns or sets the WCS option.
-------------------------------------
Getter Method
Signature
WCSOption()
Returns: Return type: NXOpen.Features.Subdivision.TransformCageDataWCSOptionType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WCSOption(wcsOption)
Parameters: wcsOption ( NXOpen.Features.Subdivision.TransformCageDataWCSOptionType
) –New in version NX9.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
Method Detail¶
ResetFallOffToLinear¶
-
TransformCageData.
ResetFallOffToLinear
¶ Resets the falloff scale to linear.
Signature
ResetFallOffToLinear()
New in version NX11.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
Validate¶
-
TransformCageData.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.