TransformCageDataTransformationMethodType Enumeration

NXOpen.Features.Subdivision.TransformCageData.TransformationMethodType is an alias for NXOpen.Features.Subdivision.TransformCageDataTransformationMethodType

class NXOpen.Features.Subdivision.TransformCageDataTransformationMethodType

Bases: object

Transformation method types

Enum Members

Enum Member Enum Member Description
Drag
Edit cage topology by direct dragging
Transform
Edit cage topology by transformations
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.