TransformCageDataScalingMethodType Enumeration

NXOpen.Features.Subdivision.TransformCageData.ScalingMethodType is an alias for NXOpen.Features.Subdivision.TransformCageDataScalingMethodType

class NXOpen.Features.Subdivision.TransformCageDataScalingMethodType

Bases: object

Scaling method

Enum Members

Enum Member Enum Member Description
Linear
Scale in the specified direction
Planar
Scale in the plane normal to specified direction
Uniform
Scale uniformly all the directions
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.