TransformCageDataMovementMethodType Enumeration¶
NXOpen.Features.Subdivision.TransformCageData.MovementMethodType is an alias for NXOpen.Features.Subdivision.TransformCageDataMovementMethodType
-
class
NXOpen.Features.Subdivision.
TransformCageDataMovementMethodType
¶ Bases:
object
Movement types
Enum Members
Enum Member Enum Member Description WCS Movement along WCS principal axis or planeView Movement in view planeVector Movement along arbitrary directionPlane Movement in arbitrary planeNormal Movement along a face normalEdge Movement along an edge-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-