AlongGuideCutBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
AlongGuideCutBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.ShipDesign.AlongGuideCut
builderTo create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateAlongGuideCutBuilder()
Default values.
Property Value DistanceTolerance 0.0254 (millimeters part), 0.001 (inches part) LeftOffsetDistance.Value 150.0 (millimeters part), 6.0 (inches part) RightOffsetDistance.Value 150.0 (millimeters part), 6.0 (inches part) New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
DistanceTolerance | Returns or sets the distance tolerance. |
GuideCurve | Returns the guide curve when the NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod is :py:class:` NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod.WeldClearance < NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod>`. |
GuideCurveList | Returns the guide curve list when the NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod is :py:class:` NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod.WeldClearance < NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod>`. |
LeftOffsetDistance | Returns the left offset distance when the NXOpen.Features.ShipDesign.AlongGuideCutBuilderWaterStopOffsetMethod is :py:class:` NXOpen.Features.ShipDesign.AlongGuideCutBuilderWaterStopOffsetMethod.Asymmetric < NXOpen.Features.ShipDesign.AlongGuideCutBuilderWaterStopOffsetMethod>`, or the offset distance for both side when the NXOpen.Features.ShipDesign.AlongGuideCutBuilderWaterStopOffsetMethod is :py:class:` NXOpen.Features.ShipDesign.AlongGuideCutBuilderWaterStopOffsetMethod.Symmetric < NXOpen.Features.ShipDesign.AlongGuideCutBuilderWaterStopOffsetMethod>`. |
ManufacturingInformation | Returns the manufacturing stock builder that holds the manufacturing data. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PlacementType | Returns or sets the method used to define the placement of the along guide cut |
RightOffsetDistance | Returns the right offset distance when the NXOpen.Features.ShipDesign.AlongGuideCutBuilderWaterStopOffsetMethod is :py:class:` NXOpen.Features.ShipDesign.AlongGuideCutBuilderWaterStopOffsetMethod.Asymmetric < NXOpen.Features.ShipDesign.AlongGuideCutBuilderWaterStopOffsetMethod>`. |
ShipStructure | Returns the target plate or stiffener when the NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod is :py:class:` NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod.WeldClearance < NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod>`. |
ShipStructureEdge | Returns the target edge when the NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod is :py:class:` NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod.WaterStop < NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod>`. |
Spreadsheet | Returns the spreadsheet builder, NXOpen.Features.ShipDesign.SteelFeatureSpreadsheetBuilder , which defines the along guide cut cross section type and parameters. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
WaterStopOffsetOption | Returns or sets the offset option when the NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod is :py:class:` NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod.WaterStop < NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod>`. |
WaterStopShape | Returns the tool object when the NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod is :py:class:` NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod.WaterStop < NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod>`. |
WaterStopShapeList | Returns the tool object list when the NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod is :py:class:` NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod.WaterStop < NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod>`. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
AlongGuideCutBuilderCreationMethod Enumeration | Creation method used to define the placement of the along guide cut |
AlongGuideCutBuilderWaterStopOffsetMethod Enumeration | Offset option used to define the placement of the water stop guide cut |
Property Detail¶
DistanceTolerance¶
-
AlongGuideCutBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance.
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
GuideCurve¶
-
AlongGuideCutBuilder.
GuideCurve
¶ Returns the guide curve when the
NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod
is :py:class:` NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod.WeldClearance < NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod>`.-------------------------------------
Getter Method
Signature
GuideCurve()
Returns: Return type: NXOpen.SelectNXObject
New in version NX8.5.0.
License requirements: None.
GuideCurveList¶
-
AlongGuideCutBuilder.
GuideCurveList
¶ Returns the guide curve list when the
NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod
is :py:class:` NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod.WeldClearance < NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod>`.-------------------------------------
Getter Method
Signature
GuideCurveList()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX11.0.0.
License requirements: None.
LeftOffsetDistance¶
-
AlongGuideCutBuilder.
LeftOffsetDistance
¶ Returns the left offset distance when the
NXOpen.Features.ShipDesign.AlongGuideCutBuilderWaterStopOffsetMethod
is :py:class:` NXOpen.Features.ShipDesign.AlongGuideCutBuilderWaterStopOffsetMethod.Asymmetric < NXOpen.Features.ShipDesign.AlongGuideCutBuilderWaterStopOffsetMethod>`, or the offset distance for both side when theNXOpen.Features.ShipDesign.AlongGuideCutBuilderWaterStopOffsetMethod
is :py:class:` NXOpen.Features.ShipDesign.AlongGuideCutBuilderWaterStopOffsetMethod.Symmetric < NXOpen.Features.ShipDesign.AlongGuideCutBuilderWaterStopOffsetMethod>`.-------------------------------------
Getter Method
Signature
LeftOffsetDistance()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
ManufacturingInformation¶
-
AlongGuideCutBuilder.
ManufacturingInformation
¶ Returns the manufacturing stock builder that holds the manufacturing data.
-------------------------------------
Getter Method
Signature
ManufacturingInformation()
Returns: Return type: NXOpen.Features.ShipDesign.ManufacturingStockBuilder
New in version NX8.5.1.
License requirements: None.
PlacementType¶
-
AlongGuideCutBuilder.
PlacementType
¶ Returns or sets the method used to define the placement of the along guide cut
-------------------------------------
Getter Method
Signature
PlacementType()
Returns: Return type: NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlacementType(placementType)
Parameters: placementType ( NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod
) –New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
RightOffsetDistance¶
-
AlongGuideCutBuilder.
RightOffsetDistance
¶ Returns the right offset distance when the
NXOpen.Features.ShipDesign.AlongGuideCutBuilderWaterStopOffsetMethod
is :py:class:` NXOpen.Features.ShipDesign.AlongGuideCutBuilderWaterStopOffsetMethod.Asymmetric < NXOpen.Features.ShipDesign.AlongGuideCutBuilderWaterStopOffsetMethod>`.-------------------------------------
Getter Method
Signature
RightOffsetDistance()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
ShipStructure¶
-
AlongGuideCutBuilder.
ShipStructure
¶ Returns the target plate or stiffener when the
NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod
is :py:class:` NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod.WeldClearance < NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod>`.-------------------------------------
Getter Method
Signature
ShipStructure()
Returns: Return type: NXOpen.SelectBodyList
New in version NX8.5.0.
License requirements: None.
ShipStructureEdge¶
-
AlongGuideCutBuilder.
ShipStructureEdge
¶ Returns the target edge when the
NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod
is :py:class:` NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod.WaterStop < NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod>`.-------------------------------------
Getter Method
Signature
ShipStructureEdge()
Returns: Return type: NXOpen.SelectEdgeList
New in version NX8.5.0.
License requirements: None.
Spreadsheet¶
-
AlongGuideCutBuilder.
Spreadsheet
¶ Returns the spreadsheet builder,
NXOpen.Features.ShipDesign.SteelFeatureSpreadsheetBuilder
, which defines the along guide cut cross section type and parameters.-------------------------------------
Getter Method
Signature
Spreadsheet()
Returns: Return type: NXOpen.Features.ShipDesign.SteelFeatureSpreadsheetBuilder
New in version NX8.5.0.
License requirements: None.
WaterStopOffsetOption¶
-
AlongGuideCutBuilder.
WaterStopOffsetOption
¶ Returns or sets the offset option when the
NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod
is :py:class:` NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod.WaterStop < NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod>`.-------------------------------------
Getter Method
Signature
WaterStopOffsetOption()
Returns: Return type: NXOpen.Features.ShipDesign.AlongGuideCutBuilderWaterStopOffsetMethod
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WaterStopOffsetOption(offsetOption)
Parameters: offsetOption ( NXOpen.Features.ShipDesign.AlongGuideCutBuilderWaterStopOffsetMethod
) –New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
WaterStopShape¶
-
AlongGuideCutBuilder.
WaterStopShape
¶ Returns the tool object when the
NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod
is :py:class:` NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod.WaterStop < NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod>`.-------------------------------------
Getter Method
Signature
WaterStopShape()
Returns: Return type: NXOpen.SelectNXObject
New in version NX8.5.0.
License requirements: None.
WaterStopShapeList¶
-
AlongGuideCutBuilder.
WaterStopShapeList
¶ Returns the tool object list when the
NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod
is :py:class:` NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod.WaterStop < NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod>`.-------------------------------------
Getter Method
Signature
WaterStopShapeList()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX11.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
AlongGuideCutBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.