AlongGuideCutBuilderCreationMethod Enumeration¶
NXOpen.Features.ShipDesign.AlongGuideCutBuilder.CreationMethod is an alias for NXOpen.Features.ShipDesign.AlongGuideCutBuilderCreationMethod
-
class
NXOpen.Features.ShipDesign.
AlongGuideCutBuilderCreationMethod
¶ Bases:
object
Creation method used to define the placement of the along guide cut
Enum Members
Enum Member Enum Member Description WeldClearance Weld clearance cut typeWaterStop Water stop cut typeEggBoxTop Egg box top cut type - added in NX11EggBoxBottom Egg box bottom cut type - added in NX11-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-