ShelfBuilder Class¶
-
class
NXOpen.Features.
ShelfBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.Shelf
builderTo create a new instance of this class, use
NXOpen.Features.AeroCollection.CreateShelfBuilder()
Default values.
Property Value DepthDimension.Value 5 (millimeters part), 0.25 (inches part) DepthMethod Offset Length1.Value 10 (millimeters part), 0.5 (inches part) Length2.Value 0 (millimeters part), 0 (inches part) LengthDimension.Value 25 (millimeters part), 1.0 (inches part) LengthMethod Full OffsetDimension.Value 0 (millimeters part), 0 (inches part) RampLength1.Value 10 (millimeters part), 0.5 (inches part) RampLength2.Value 10 (millimeters part), 0.5 (inches part) RefType1 Face RefType2 Face ShelfType End StepMethod1 Normal StepMethod2 Normal WidthDimension.Value 5 (millimeters part), 0.25 (inches part) New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
DepthDimension | Returns the depth dimension |
DepthMethod | Returns or sets the depth method |
Length1 | Returns the length1 |
Length2 | Returns the length2 |
LengthDimension | Returns the length dimension |
LengthMethod | Returns or sets the length method |
LimitCurve1 | Returns the limit curve1 |
LimitCurve2 | Returns the limit curve2 |
LimitFace1 | Returns the limit face1 |
LimitFace2 | Returns the limit face2 |
LimitPlane1 | Returns or sets the limit plane1 |
LimitPlane2 | Returns or sets the limit plane2 |
LimitPoint1 | Returns or sets the limit point1 |
LimitPoint2 | Returns or sets the limit point2 |
OffsetDimension | Returns the offset dimension |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ProjectionDir1 | Returns the project direction 1 |
ProjectionDir2 | Returns the project direction 2 |
RampLength1 | Returns the ramp length1 |
RampLength2 | Returns the ramp length2 |
RefType1 | Returns or sets the ref type1 |
RefType2 | Returns or sets the ref type2 |
ReverseDepthDirection | Returns or sets whether reverse depth direction |
ReverseWidthDirection | Returns or sets whether reverse width direction |
Selectface | Returns the selected face |
ShelfEdge | Returns the shelf edge |
ShelfEnd | Returns or sets the shelf end |
ShelfType | Returns or sets the type |
StepMethod1 | Returns or sets the step method1 |
StepMethod2 | Returns or sets the step method2 |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Swap | Returns or sets the swap |
Tag | Returns the Tag for this object. |
WidthDimension | Returns the width dimension |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ShelfBuilderDepthMethods Enumeration | Depth Method for Depth Face |
ShelfBuilderLengthMethods Enumeration | Depth Method for Length |
ShelfBuilderReferenceType Enumeration | Type of Reference Object |
ShelfBuilderStepMethod Enumeration | Step Method for Side Face |
ShelfBuilderTypes Enumeration | Type of shelf. |
Property Detail¶
DepthDimension¶
-
ShelfBuilder.
DepthDimension
¶ Returns the depth dimension
-------------------------------------
Getter Method
Signature
DepthDimension()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
DepthMethod¶
-
ShelfBuilder.
DepthMethod
¶ Returns or sets the depth method
-------------------------------------
Getter Method
Signature
DepthMethod()
Returns: Return type: NXOpen.Features.ShelfBuilderDepthMethods
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DepthMethod(depthMethod)
Parameters: depthMethod ( NXOpen.Features.ShelfBuilderDepthMethods
) –New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
Length1¶
-
ShelfBuilder.
Length1
¶ Returns the length1
-------------------------------------
Getter Method
Signature
Length1()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
Length2¶
-
ShelfBuilder.
Length2
¶ Returns the length2
-------------------------------------
Getter Method
Signature
Length2()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
LengthDimension¶
-
ShelfBuilder.
LengthDimension
¶ Returns the length dimension
-------------------------------------
Getter Method
Signature
LengthDimension()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
LengthMethod¶
-
ShelfBuilder.
LengthMethod
¶ Returns or sets the length method
-------------------------------------
Getter Method
Signature
LengthMethod()
Returns: Return type: NXOpen.Features.ShelfBuilderLengthMethods
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LengthMethod(lengthMethod)
Parameters: lengthMethod ( NXOpen.Features.ShelfBuilderLengthMethods
) –New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
LimitCurve1¶
-
ShelfBuilder.
LimitCurve1
¶ Returns the limit curve1
-------------------------------------
Getter Method
Signature
LimitCurve1()
Returns: Return type: NXOpen.Section
New in version NX10.0.0.
License requirements: None.
LimitCurve2¶
-
ShelfBuilder.
LimitCurve2
¶ Returns the limit curve2
-------------------------------------
Getter Method
Signature
LimitCurve2()
Returns: Return type: NXOpen.Section
New in version NX10.0.0.
License requirements: None.
LimitFace1¶
-
ShelfBuilder.
LimitFace1
¶ Returns the limit face1
-------------------------------------
Getter Method
Signature
LimitFace1()
Returns: Return type: NXOpen.ScCollector
New in version NX10.0.0.
License requirements: None.
LimitFace2¶
-
ShelfBuilder.
LimitFace2
¶ Returns the limit face2
-------------------------------------
Getter Method
Signature
LimitFace2()
Returns: Return type: NXOpen.ScCollector
New in version NX10.0.0.
License requirements: None.
LimitPlane1¶
-
ShelfBuilder.
LimitPlane1
¶ Returns or sets the limit plane1
-------------------------------------
Getter Method
Signature
LimitPlane1()
Returns: Return type: NXOpen.Plane
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LimitPlane1(limitPlane1)
Parameters: limitPlane1 ( NXOpen.Plane
) –New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
LimitPlane2¶
-
ShelfBuilder.
LimitPlane2
¶ Returns or sets the limit plane2
-------------------------------------
Getter Method
Signature
LimitPlane2()
Returns: Return type: NXOpen.Plane
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LimitPlane2(limitPlane2)
Parameters: limitPlane2 ( NXOpen.Plane
) –New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
LimitPoint1¶
-
ShelfBuilder.
LimitPoint1
¶ Returns or sets the limit point1
-------------------------------------
Getter Method
Signature
LimitPoint1()
Returns: Return type: NXOpen.Point
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LimitPoint1(limitPoint1)
Parameters: limitPoint1 ( NXOpen.Point
) –New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
LimitPoint2¶
-
ShelfBuilder.
LimitPoint2
¶ Returns or sets the limit point2
-------------------------------------
Getter Method
Signature
LimitPoint2()
Returns: Return type: NXOpen.Point
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LimitPoint2(limitPoint2)
Parameters: limitPoint2 ( NXOpen.Point
) –New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
OffsetDimension¶
-
ShelfBuilder.
OffsetDimension
¶ Returns the offset dimension
-------------------------------------
Getter Method
Signature
OffsetDimension()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
ProjectionDir1¶
-
ShelfBuilder.
ProjectionDir1
¶ Returns the project direction 1
-------------------------------------
Getter Method
Signature
ProjectionDir1()
Returns: Projection Options data Return type: NXOpen.GeometricUtilities.ProjectionOptions
New in version NX10.0.0.
License requirements: None.
ProjectionDir2¶
-
ShelfBuilder.
ProjectionDir2
¶ Returns the project direction 2
-------------------------------------
Getter Method
Signature
ProjectionDir2()
Returns: Projection Options data Return type: NXOpen.GeometricUtilities.ProjectionOptions
New in version NX10.0.0.
License requirements: None.
RampLength1¶
-
ShelfBuilder.
RampLength1
¶ Returns the ramp length1
-------------------------------------
Getter Method
Signature
RampLength1()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
RampLength2¶
-
ShelfBuilder.
RampLength2
¶ Returns the ramp length2
-------------------------------------
Getter Method
Signature
RampLength2()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
RefType1¶
-
ShelfBuilder.
RefType1
¶ Returns or sets the ref type1
-------------------------------------
Getter Method
Signature
RefType1()
Returns: Return type: NXOpen.Features.ShelfBuilderReferenceType
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RefType1(refType1)
Parameters: refType1 ( NXOpen.Features.ShelfBuilderReferenceType
) –New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
RefType2¶
-
ShelfBuilder.
RefType2
¶ Returns or sets the ref type2
-------------------------------------
Getter Method
Signature
RefType2()
Returns: Return type: NXOpen.Features.ShelfBuilderReferenceType
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RefType2(refType2)
Parameters: refType2 ( NXOpen.Features.ShelfBuilderReferenceType
) –New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
ReverseDepthDirection¶
-
ShelfBuilder.
ReverseDepthDirection
¶ Returns or sets whether reverse depth direction
-------------------------------------
Getter Method
Signature
ReverseDepthDirection()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseDepthDirection(reverseDepthDirection)
Parameters: reverseDepthDirection (bool) – New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
ReverseWidthDirection¶
-
ShelfBuilder.
ReverseWidthDirection
¶ Returns or sets whether reverse width direction
-------------------------------------
Getter Method
Signature
ReverseWidthDirection()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseWidthDirection(reverseWidthDirection)
Parameters: reverseWidthDirection (bool) – New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
Selectface¶
-
ShelfBuilder.
Selectface
¶ Returns the selected face
-------------------------------------
Getter Method
Signature
Selectface()
Returns: Return type: NXOpen.ScCollector
New in version NX10.0.0.
License requirements: None.
ShelfEdge¶
-
ShelfBuilder.
ShelfEdge
¶ Returns the shelf edge
-------------------------------------
Getter Method
Signature
ShelfEdge()
Returns: Return type: NXOpen.ScCollector
New in version NX10.0.0.
License requirements: None.
ShelfEnd¶
-
ShelfBuilder.
ShelfEnd
¶ Returns or sets the shelf end
-------------------------------------
Getter Method
Signature
ShelfEnd()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShelfEnd(shelfEnd)
Parameters: shelfEnd (bool) – New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
ShelfType¶
-
ShelfBuilder.
ShelfType
¶ Returns or sets the type
-------------------------------------
Getter Method
Signature
ShelfType()
Returns: Return type: NXOpen.Features.ShelfBuilderTypes
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShelfType(type)
Parameters: type ( NXOpen.Features.ShelfBuilderTypes
) –New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
StepMethod1¶
-
ShelfBuilder.
StepMethod1
¶ Returns or sets the step method1
-------------------------------------
Getter Method
Signature
StepMethod1()
Returns: Return type: NXOpen.Features.ShelfBuilderStepMethod
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StepMethod1(stepMethod1)
Parameters: stepMethod1 ( NXOpen.Features.ShelfBuilderStepMethod
) –New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
StepMethod2¶
-
ShelfBuilder.
StepMethod2
¶ Returns or sets the step method2
-------------------------------------
Getter Method
Signature
StepMethod2()
Returns: Return type: NXOpen.Features.ShelfBuilderStepMethod
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StepMethod2(stepMethod2)
Parameters: stepMethod2 ( NXOpen.Features.ShelfBuilderStepMethod
) –New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
Swap¶
-
ShelfBuilder.
Swap
¶ Returns or sets the swap
-------------------------------------
Getter Method
Signature
Swap()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Swap(swap)
Parameters: swap (bool) – New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
WidthDimension¶
-
ShelfBuilder.
WidthDimension
¶ Returns the width dimension
-------------------------------------
Getter Method
Signature
WidthDimension()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
ShelfBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.