ShelfBuilderTypes Enumeration

NXOpen.Features.ShelfBuilder.Types is an alias for NXOpen.Features.ShelfBuilderTypes

class NXOpen.Features.ShelfBuilderTypes

Bases: object

Type of shelf.

It has end and middle type

Enum Members

Enum Member Enum Member Description
End
Middle
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.