CircularBlendCurveBuilder Class¶
-
class
NXOpen.Features.
CircularBlendCurveBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.CircularBlendCurve
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateCircularBlendCurveBuilder()
Default values.
Property Value Associative True CurveFitMethod.FitOption Cubic CurveFitMethod.MaximumDegree 7 CurveFitMethod.MaximumSegments 1 CylinderRadius.Value 0.0 (millimeters part), 0.0 (inches part) DirectionOption BestFit PointArclength.Expression.Value 0.0 (millimeters part), 0.0 (inches part) RadiusOption PointOnFirstCurve ShapeControlFirstCurve 2.0 ShapeControlSecondCurve 2.0 New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Associative | Returns or sets whether to create the associative output or non associative output |
CurveFitMethod | Returns the curve fit method as NXOpen.GeometricUtilities.CurveFitOptions |
CylinderRadius | Returns the cylinder radius as NXOpen.Expression , if NXOpen.Features.CircularBlendCurveBuilderCylinderRadiusOption is NXOpen.Features.CircularBlendCurveBuilderCylinderRadiusOption.Value |
DirectionOption | Returns or sets the cylinder direction option as NXOpen.Features.CircularBlendCurveBuilderCylinderDirectionOption |
DistanceTolerance | Returns or sets the distance tolerance |
FirstCurve | Returns the first curve chain |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PointArclength | Returns the location of the point on curve as arclength or %arclength, if NXOpen.Features.CircularBlendCurveBuilderCylinderRadiusOption is NXOpen.Features.CircularBlendCurveBuilderCylinderRadiusOption.PointOnFirstCurve or Features.CircularBlendCurveBuilderCylinderRadiusOption.PointOnSecondCurve |
RadiusOption | Returns or sets the cylinder radius option as NXOpen.Features.CircularBlendCurveBuilderCylinderRadiusOption |
SecondCurve | Returns the second curve chain |
ShapeControlFirstCurve | Returns or sets the shape control for first curve, specifies how quickly the circular blend curve deviates from the first curve. |
ShapeControlSecondCurve | Returns or sets the shape control for second curve, specifies how quickly the circular blend curve deviates from the second curve. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Vector | Returns or sets the vector for cylinder direction, if NXOpen.Features.CircularBlendCurveBuilderCylinderDirectionOption is NXOpen.Features.CircularBlendCurveBuilderCylinderDirectionOption.Vector |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
ComplementArc | Complements the circular blend curve |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
Evaluate | Evaluates the circular blend curve |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CircularBlendCurveBuilderCylinderDirectionOption Enumeration | Represents the cylinder direction options |
CircularBlendCurveBuilderCylinderRadiusOption Enumeration | Represents the cylinder radius options |
Property Detail¶
Associative¶
-
CircularBlendCurveBuilder.
Associative
¶ Returns or sets whether to create the associative output or non associative output
-------------------------------------
Getter Method
Signature
Associative()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Associative(associative)
Parameters: associative (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
CurveFitMethod¶
-
CircularBlendCurveBuilder.
CurveFitMethod
¶ Returns the curve fit method as
NXOpen.GeometricUtilities.CurveFitOptions
-------------------------------------
Getter Method
Signature
CurveFitMethod()
Returns: Return type: NXOpen.GeometricUtilities.CurveFitOptions
New in version NX5.0.0.
License requirements: None.
CylinderRadius¶
-
CircularBlendCurveBuilder.
CylinderRadius
¶ Returns the cylinder radius as
NXOpen.Expression
, ifNXOpen.Features.CircularBlendCurveBuilderCylinderRadiusOption
isNXOpen.Features.CircularBlendCurveBuilderCylinderRadiusOption.Value
-------------------------------------
Getter Method
Signature
CylinderRadius()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
DirectionOption¶
-
CircularBlendCurveBuilder.
DirectionOption
¶ Returns or sets the cylinder direction option as
NXOpen.Features.CircularBlendCurveBuilderCylinderDirectionOption
-------------------------------------
Getter Method
Signature
DirectionOption()
Returns: Return type: NXOpen.Features.CircularBlendCurveBuilderCylinderDirectionOption
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DirectionOption(directionOption)
Parameters: directionOption ( NXOpen.Features.CircularBlendCurveBuilderCylinderDirectionOption
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
DistanceTolerance¶
-
CircularBlendCurveBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
FirstCurve¶
-
CircularBlendCurveBuilder.
FirstCurve
¶ Returns the first curve chain
-------------------------------------
Getter Method
Signature
FirstCurve()
Returns: Return type: NXOpen.Section
New in version NX5.0.0.
License requirements: None.
PointArclength¶
-
CircularBlendCurveBuilder.
PointArclength
¶ Returns the location of the point on curve as arclength or %arclength, if
NXOpen.Features.CircularBlendCurveBuilderCylinderRadiusOption
isNXOpen.Features.CircularBlendCurveBuilderCylinderRadiusOption.PointOnFirstCurve
orFeatures.CircularBlendCurveBuilderCylinderRadiusOption.PointOnSecondCurve
-------------------------------------
Getter Method
Signature
PointArclength()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX5.0.0.
License requirements: None.
RadiusOption¶
-
CircularBlendCurveBuilder.
RadiusOption
¶ Returns or sets the cylinder radius option as
NXOpen.Features.CircularBlendCurveBuilderCylinderRadiusOption
-------------------------------------
Getter Method
Signature
RadiusOption()
Returns: Return type: NXOpen.Features.CircularBlendCurveBuilderCylinderRadiusOption
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RadiusOption(radiusOption)
Parameters: radiusOption ( NXOpen.Features.CircularBlendCurveBuilderCylinderRadiusOption
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SecondCurve¶
-
CircularBlendCurveBuilder.
SecondCurve
¶ Returns the second curve chain
-------------------------------------
Getter Method
Signature
SecondCurve()
Returns: Return type: NXOpen.Section
New in version NX5.0.0.
License requirements: None.
ShapeControlFirstCurve¶
-
CircularBlendCurveBuilder.
ShapeControlFirstCurve
¶ Returns or sets the shape control for first curve, specifies how quickly the circular blend curve deviates from the first curve.
The lower the number, the quicker the deviation.
-------------------------------------
Getter Method
Signature
ShapeControlFirstCurve()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShapeControlFirstCurve(shapeControlCurve1)
Parameters: shapeControlCurve1 (float) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ShapeControlSecondCurve¶
-
CircularBlendCurveBuilder.
ShapeControlSecondCurve
¶ Returns or sets the shape control for second curve, specifies how quickly the circular blend curve deviates from the second curve.
The lower the number, the quicker the deviation.
-------------------------------------
Getter Method
Signature
ShapeControlSecondCurve()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShapeControlSecondCurve(shapeControlCurve2)
Parameters: shapeControlCurve2 (float) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Vector¶
-
CircularBlendCurveBuilder.
Vector
¶ Returns or sets the vector for cylinder direction, if
NXOpen.Features.CircularBlendCurveBuilderCylinderDirectionOption
isNXOpen.Features.CircularBlendCurveBuilderCylinderDirectionOption.Vector
-------------------------------------
Getter Method
Signature
Vector()
Returns: Return type: NXOpen.Direction
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Vector(vector)
Parameters: vector ( NXOpen.Direction
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
ComplementArc¶
-
CircularBlendCurveBuilder.
ComplementArc
¶ Complements the circular blend curve
Signature
ComplementArc()
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Evaluate¶
-
CircularBlendCurveBuilder.
Evaluate
¶ Evaluates the circular blend curve
Signature
Evaluate()
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Validate¶
-
CircularBlendCurveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.