CircularBlendCurveBuilderCylinderRadiusOption Enumeration

NXOpen.Features.CircularBlendCurveBuilder.CylinderRadiusOption is an alias for NXOpen.Features.CircularBlendCurveBuilderCylinderRadiusOption

class NXOpen.Features.CircularBlendCurveBuilderCylinderRadiusOption

Bases: object

Represents the cylinder radius options

Enum Members

Enum Member Enum Member Description
PointOnFirstCurve
Radius by point on first curve
PointOnSecondCurve
Radius by point on second curve
Value
Radius by value
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.