CircularBlendCurveBuilderCylinderDirectionOption Enumeration

NXOpen.Features.CircularBlendCurveBuilder.CylinderDirectionOption is an alias for NXOpen.Features.CircularBlendCurveBuilderCylinderDirectionOption

class NXOpen.Features.CircularBlendCurveBuilderCylinderDirectionOption

Bases: object

Represents the cylinder direction options

Enum Members

Enum Member Enum Member Description
BestFit
Best fit method
Variable
Variable method
Vector
Specify vector method
CurrentView
Current view method
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.