AeroFlangeBuilder Class¶
-
class
NXOpen.Features.
AeroFlangeBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.AeroFlange
builderTo create a new instance of this class, use
NXOpen.Features.AeroCollection.CreateAeroFlangeBuilder()
Default values.
Property Value BooleanOperation.Type Create GuideObjectType Face Limit1Offset.Value 0 (millimeters part), 0 (inches part) Limit1Type FromGuideCurve Limit2Offset.Value 0 (millimeters part), 0 (inches part) Limit2Type FromGuideCurve Thickness.Value 2 (millimeters part), 0.1 (inches part) ThicknessDimensionType Simple ThicknessOffset.Value 0 (millimeters part), 0 (inches part) Width1.Value 25 (millimeters part), 1 (inches part) Width2.Value 25 (millimeters part), 1 (inches part) WidthDimensionType Simple WidthMethod OffsetGuideCurveAlongSkin New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
BooleanOperation | Returns the boolean operation |
GuideFaces | Returns the guide faces |
GuideObjectType | Returns or sets the guide object type |
IsLimit1MeasureExpressionUsed | Returns or sets the flag of whether limit1 measure expression used |
IsLimit2MeasureExpressionUsed | Returns or sets the flag of whether limit2 measure expression used |
Limit1Offset | Returns the limit1 offset |
Limit1Point | Returns the limit1 point |
Limit1Selection | Returns the limit1 selection |
Limit1Type | Returns or sets the limit1 type |
Limit2Offset | Returns the limit2 offset |
Limit2Point | Returns the limit2 point |
Limit2Selection | Returns the limit2 selection |
Limit2Type | Returns or sets the limit2 type |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Plane | Returns or sets the plane |
ProjectDirection | Returns the project direction |
ReverseLimit1OffsetDirection | Returns or sets the reverse limit1 offset direction flag. |
ReverseLimit2OffsetDirection | Returns or sets the reverse limit2 offset direction flag. |
ReverseThicknessDirection | Returns or sets the reverse thickness direction flag. |
ReverseThicknessOffsetDirection | Returns or sets the reverse thickness offset direction flag. |
ReverseWidth1Direction | Returns or sets the reverse width1 direction flag. |
ReverseWidth2Direction | Returns or sets the reverse width2 direction flag. |
Section | Returns the section |
SkinFaceCollector | Returns the skin face collector |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Thickness | Returns the thickness |
ThicknessDimensionType | Returns or sets the thickness dimension type |
ThicknessOffset | Returns the thickness offset |
Width1 | Returns the width1 |
Width2 | Returns the width2 |
WidthDimensionType | Returns or sets the width dimension type |
WidthMethod | Returns or sets the width method |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
AeroFlangeBuilderGuideObjectTypes Enumeration | This attribute represents the Guide Object types |
AeroFlangeBuilderLimitObjectTypes Enumeration | This attribute represents the limit object types |
AeroFlangeBuilderPointOption Enumeration | This attribute represents the options for on path dimension |
AeroFlangeBuilderThicknessDimensionOptions Enumeration | This attribute represents the options for thickness dimension |
AeroFlangeBuilderWidthDimensionOptions Enumeration | This attribute represents the options for width dimension |
AeroFlangeBuilderWidthMethods Enumeration | This attribute represents the width method |
Property Detail¶
BooleanOperation¶
-
AeroFlangeBuilder.
BooleanOperation
¶ Returns the boolean operation
-------------------------------------
Getter Method
Signature
BooleanOperation()
Returns: Return type: NXOpen.GeometricUtilities.BooleanOperation
New in version NX11.0.0.
License requirements: None.
GuideFaces¶
-
AeroFlangeBuilder.
GuideFaces
¶ Returns the guide faces
-------------------------------------
Getter Method
Signature
GuideFaces()
Returns: Return type: NXOpen.ScCollector
New in version NX10.0.0.
License requirements: None.
GuideObjectType¶
-
AeroFlangeBuilder.
GuideObjectType
¶ Returns or sets the guide object type
-------------------------------------
Getter Method
Signature
GuideObjectType()
Returns: Return type: NXOpen.Features.AeroFlangeBuilderGuideObjectTypes
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GuideObjectType(guideObjectType)
Parameters: guideObjectType ( NXOpen.Features.AeroFlangeBuilderGuideObjectTypes
) –New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
IsLimit1MeasureExpressionUsed¶
-
AeroFlangeBuilder.
IsLimit1MeasureExpressionUsed
¶ Returns or sets the flag of whether limit1 measure expression used
-------------------------------------
Getter Method
Signature
IsLimit1MeasureExpressionUsed()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsLimit1MeasureExpressionUsed(isLimit1MeasureExpressionUsed)
Parameters: isLimit1MeasureExpressionUsed (bool) – New in version NX11.0.0.
License requirements: None.
IsLimit2MeasureExpressionUsed¶
-
AeroFlangeBuilder.
IsLimit2MeasureExpressionUsed
¶ Returns or sets the flag of whether limit2 measure expression used
-------------------------------------
Getter Method
Signature
IsLimit2MeasureExpressionUsed()
Returns: Return type: bool New in version NX11.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
-------------------------------------
Setter Method
Signature
IsLimit2MeasureExpressionUsed(isLimit2MeasureExpressionUsed)
Parameters: isLimit2MeasureExpressionUsed (bool) – New in version NX11.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
Limit1Offset¶
-
AeroFlangeBuilder.
Limit1Offset
¶ Returns the limit1 offset
-------------------------------------
Getter Method
Signature
Limit1Offset()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
Limit1Point¶
-
AeroFlangeBuilder.
Limit1Point
¶ Returns the limit1 point
-------------------------------------
Getter Method
Signature
Limit1Point()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX11.0.0.
License requirements: None.
Limit1Selection¶
-
AeroFlangeBuilder.
Limit1Selection
¶ Returns the limit1 selection
-------------------------------------
Getter Method
Signature
Limit1Selection()
Returns: Return type: NXOpen.ScCollector
New in version NX11.0.0.
License requirements: None.
Limit1Type¶
-
AeroFlangeBuilder.
Limit1Type
¶ Returns or sets the limit1 type
-------------------------------------
Getter Method
Signature
Limit1Type()
Returns: Return type: NXOpen.Features.AeroFlangeBuilderLimitObjectTypes
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Limit1Type(limit1Type)
Parameters: limit1Type ( NXOpen.Features.AeroFlangeBuilderLimitObjectTypes
) –New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
Limit2Offset¶
-
AeroFlangeBuilder.
Limit2Offset
¶ Returns the limit2 offset
-------------------------------------
Getter Method
Signature
Limit2Offset()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
Limit2Point¶
-
AeroFlangeBuilder.
Limit2Point
¶ Returns the limit2 point
-------------------------------------
Getter Method
Signature
Limit2Point()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX11.0.0.
License requirements: None.
Limit2Selection¶
-
AeroFlangeBuilder.
Limit2Selection
¶ Returns the limit2 selection
-------------------------------------
Getter Method
Signature
Limit2Selection()
Returns: Return type: NXOpen.ScCollector
New in version NX10.0.0.
License requirements: None.
Limit2Type¶
-
AeroFlangeBuilder.
Limit2Type
¶ Returns or sets the limit2 type
-------------------------------------
Getter Method
Signature
Limit2Type()
Returns: Return type: NXOpen.Features.AeroFlangeBuilderLimitObjectTypes
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Limit2Type(limit2Type)
Parameters: limit2Type ( NXOpen.Features.AeroFlangeBuilderLimitObjectTypes
) –New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
Plane¶
-
AeroFlangeBuilder.
Plane
¶ Returns or sets the plane
-------------------------------------
Getter Method
Signature
Plane()
Returns: Return type: NXOpen.Plane
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Plane(plane)
Parameters: plane ( NXOpen.Plane
) –New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
ProjectDirection¶
-
AeroFlangeBuilder.
ProjectDirection
¶ Returns the project direction
-------------------------------------
Getter Method
Signature
ProjectDirection()
Returns: Projection Options data Return type: NXOpen.GeometricUtilities.ProjectionOptions
New in version NX11.0.0.
License requirements: None.
ReverseLimit1OffsetDirection¶
-
AeroFlangeBuilder.
ReverseLimit1OffsetDirection
¶ Returns or sets the reverse limit1 offset direction flag.
Indicates whether the limit1 offset direction has been flipped from its initial inferred direction
-------------------------------------
Getter Method
Signature
ReverseLimit1OffsetDirection()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseLimit1OffsetDirection(reverseLimit1OffsetDirection)
Parameters: reverseLimit1OffsetDirection (bool) – New in version NX11.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
ReverseLimit2OffsetDirection¶
-
AeroFlangeBuilder.
ReverseLimit2OffsetDirection
¶ Returns or sets the reverse limit2 offset direction flag.
Indicates whether the limit2 offset direction has been flipped from its initial inferred direction
-------------------------------------
Getter Method
Signature
ReverseLimit2OffsetDirection()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseLimit2OffsetDirection(reverseLimit2OffsetDirection)
Parameters: reverseLimit2OffsetDirection (bool) – New in version NX11.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
ReverseThicknessDirection¶
-
AeroFlangeBuilder.
ReverseThicknessDirection
¶ Returns or sets the reverse thickness direction flag.
Indicates whether the thickness direction has been flipped from its initial inferred direction
-------------------------------------
Getter Method
Signature
ReverseThicknessDirection()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseThicknessDirection(reverseThicknessDirection)
Parameters: reverseThicknessDirection (bool) – New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
ReverseThicknessOffsetDirection¶
-
AeroFlangeBuilder.
ReverseThicknessOffsetDirection
¶ Returns or sets the reverse thickness offset direction flag.
Indicates whether the thickness offset direction has been flipped from its initial inferred direction
-------------------------------------
Getter Method
Signature
ReverseThicknessOffsetDirection()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseThicknessOffsetDirection(reverseThicknessOffsetDirection)
Parameters: reverseThicknessOffsetDirection (bool) – New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
ReverseWidth1Direction¶
-
AeroFlangeBuilder.
ReverseWidth1Direction
¶ Returns or sets the reverse width1 direction flag.
Indicates whether the width1 direction has been flipped from its initial inferred direction
-------------------------------------
Getter Method
Signature
ReverseWidth1Direction()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseWidth1Direction(reverseWidth1Direction)
Parameters: reverseWidth1Direction (bool) – New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
ReverseWidth2Direction¶
-
AeroFlangeBuilder.
ReverseWidth2Direction
¶ Returns or sets the reverse width2 direction flag.
Indicates whether the width2 direction has been flipped from its initial inferred direction
-------------------------------------
Getter Method
Signature
ReverseWidth2Direction()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseWidth2Direction(reverseWidth2Direction)
Parameters: reverseWidth2Direction (bool) – New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
Section¶
-
AeroFlangeBuilder.
Section
¶ Returns the section
-------------------------------------
Getter Method
Signature
Section()
Returns: Return type: NXOpen.Section
New in version NX10.0.0.
License requirements: None.
SkinFaceCollector¶
-
AeroFlangeBuilder.
SkinFaceCollector
¶ Returns the skin face collector
-------------------------------------
Getter Method
Signature
SkinFaceCollector()
Returns: Return type: NXOpen.ScCollector
New in version NX10.0.0.
License requirements: None.
Thickness¶
-
AeroFlangeBuilder.
Thickness
¶ Returns the thickness
-------------------------------------
Getter Method
Signature
Thickness()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
ThicknessDimensionType¶
-
AeroFlangeBuilder.
ThicknessDimensionType
¶ Returns or sets the thickness dimension type
-------------------------------------
Getter Method
Signature
ThicknessDimensionType()
Returns: Return type: NXOpen.Features.AeroFlangeBuilderThicknessDimensionOptions
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ThicknessDimensionType(thicknessDimensionType)
Parameters: thicknessDimensionType ( NXOpen.Features.AeroFlangeBuilderThicknessDimensionOptions
) –New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
ThicknessOffset¶
-
AeroFlangeBuilder.
ThicknessOffset
¶ Returns the thickness offset
-------------------------------------
Getter Method
Signature
ThicknessOffset()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
Width1¶
-
AeroFlangeBuilder.
Width1
¶ Returns the width1
-------------------------------------
Getter Method
Signature
Width1()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
Width2¶
-
AeroFlangeBuilder.
Width2
¶ Returns the width2
-------------------------------------
Getter Method
Signature
Width2()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
WidthDimensionType¶
-
AeroFlangeBuilder.
WidthDimensionType
¶ Returns or sets the width dimension type
-------------------------------------
Getter Method
Signature
WidthDimensionType()
Returns: Return type: NXOpen.Features.AeroFlangeBuilderWidthDimensionOptions
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WidthDimensionType(widthDimensionType)
Parameters: widthDimensionType ( NXOpen.Features.AeroFlangeBuilderWidthDimensionOptions
) –New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
WidthMethod¶
-
AeroFlangeBuilder.
WidthMethod
¶ Returns or sets the width method
-------------------------------------
Getter Method
Signature
WidthMethod()
Returns: Return type: NXOpen.Features.AeroFlangeBuilderWidthMethods
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WidthMethod(widthMethod)
Parameters: widthMethod ( NXOpen.Features.AeroFlangeBuilderWidthMethods
) –New in version NX10.0.0.
License requirements: nx_aero_design (” NX Aero Design”)
Method Detail¶
Validate¶
-
AeroFlangeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.