PierceTaskBuilder Class¶
-
class
NXOpen.Die.
PierceTaskBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Pierce Task feature builder
To create a new instance of this class, use
NXOpen.Die.DieCollection.PierceTask()
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the angle tolerance of the pierce task |
AssociatedObjects | Returns the assoc objects |
CamDirection | Returns or sets the cam direction of the pierce task |
CamType | Returns or sets the cam type of the pierce task |
CenterPointOption | Returns or sets the center point output option of the pierce task |
CreateScrap | Returns or sets the create scrap setting of the pierce task. |
DistanceTolerance | Returns or sets the distance tolerance of the pierce task |
FinishOperation | Returns or sets the finish operation of the pierce task True indicates the pierce is to be a finish pierce. |
LayoutFlange | Returns or sets the layout flange setting of the pierce task. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PierceHoles | Returns the pierce holes |
PierceHolesList | Returns the pierce holes list |
PrecisionType | Returns or sets the precision type of the pierce task |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TipFeature | Returns the tip feature |
TippedProduct | Returns or sets the tipped product of the pierce task |
TrimNewDieFace | Returns or sets the trim new die face, from NX10. |
WithoutWorkflowSheet | Returns or sets the without workflow sheet of the pierce task builder. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAssociativeObjects | Gets the associative objects of the pierce task @return |
GetCameraLayerAndXmlp | Gets the camera layer settings and xmlp data @return 1 layer setting string for each camera object. |
GetCameraNames | Gets the names of the camera @return each string contains the name of a camera object |
GetCameraViews | Gets the camera views of the pierce task @return |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDetails | Gets the detailed description of the pierce task @return detail strings |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
GetPierceBounds | Gets the pierce bounds of the pierce task @return Profile entries that make up the boundary of the pierce task |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
NewPierceHole | Creates a new pierce hole item in the set @return |
SetAssociativeObjects | Sets the associative objects of the pierce task |
SetCameraLayerAndXmlp | Sets the camera layer settings and xmlp data |
SetCameraNames | Sets the names of the camera |
SetCameraViews | Sets the camera views of the pierce task |
SetDetails | Sets the detailed description of the pierce task |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetPierceBounds | Sets the pierce bounds of the pierce task. |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PierceTaskBuilderCamTypes Enumeration | Settings for the cam type of the pierce task. |
PierceTaskBuilderCenterPointOptionTypes Enumeration | Settings for the center point output options of the pierce task. |
PierceTaskBuilderPrecisionTypes Enumeration | Settings for the precistion type of the pierce task. |
Property Detail¶
AngleTolerance¶
-
PierceTaskBuilder.
AngleTolerance
¶ Returns or sets the angle tolerance of the pierce task
-------------------------------------
Getter Method
Signature
AngleTolerance()
Returns: Return type: float New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
AngleTolerance(angleTolerance)
Parameters: angleTolerance (float) – New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
AssociatedObjects¶
-
PierceTaskBuilder.
AssociatedObjects
¶ Returns the assoc objects
-------------------------------------
Getter Method
Signature
AssociatedObjects()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX5.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
CamDirection¶
-
PierceTaskBuilder.
CamDirection
¶ Returns or sets the cam direction of the pierce task
-------------------------------------
Getter Method
Signature
CamDirection()
Returns: Return type: NXOpen.ILocation
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
CamDirection(camDirection)
Parameters: camDirection ( NXOpen.ILocation
) –New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
CamType¶
-
PierceTaskBuilder.
CamType
¶ Returns or sets the cam type of the pierce task
-------------------------------------
Getter Method
Signature
CamType()
Returns: Return type: NXOpen.Die.PierceTaskBuilderCamTypes
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
CamType(camType)
Parameters: camType ( NXOpen.Die.PierceTaskBuilderCamTypes
) –New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
CenterPointOption¶
-
PierceTaskBuilder.
CenterPointOption
¶ Returns or sets the center point output option of the pierce task
-------------------------------------
Getter Method
Signature
CenterPointOption()
Returns: Return type: NXOpen.Die.PierceTaskBuilderCenterPointOptionTypes
New in version NX5.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
CenterPointOption(centerPointOption)
Parameters: centerPointOption ( NXOpen.Die.PierceTaskBuilderCenterPointOptionTypes
) –New in version NX5.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
CreateScrap¶
-
PierceTaskBuilder.
CreateScrap
¶ Returns or sets the create scrap setting of the pierce task.
True indicates that the scrap is to be created.
-------------------------------------
Getter Method
Signature
CreateScrap()
Returns: Return type: bool New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
CreateScrap(createScrap)
Parameters: createScrap (bool) – New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”)
DistanceTolerance¶
-
PierceTaskBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance of the pierce task
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
FinishOperation¶
-
PierceTaskBuilder.
FinishOperation
¶ Returns or sets the finish operation of the pierce task True indicates the pierce is to be a finish pierce.
False indicates rough pierce.
-------------------------------------
Getter Method
Signature
FinishOperation()
Returns: Return type: bool New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
FinishOperation(finishOperation)
Parameters: finishOperation (bool) – New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
LayoutFlange¶
-
PierceTaskBuilder.
LayoutFlange
¶ Returns or sets the layout flange setting of the pierce task.
True indicates that the pierce curve is to be laid out on the flange.
-------------------------------------
Getter Method
Signature
LayoutFlange()
Returns: Return type: bool New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
LayoutFlange(layoutFlange)
Parameters: layoutFlange (bool) – New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
PierceHoles¶
-
PierceTaskBuilder.
PierceHoles
¶ Returns the pierce holes
-------------------------------------
Getter Method
Signature
PierceHoles()
Returns: Return type: NXOpen.ScCollector
New in version NX5.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
PierceHolesList¶
-
PierceTaskBuilder.
PierceHolesList
¶ Returns the pierce holes list
-------------------------------------
Getter Method
Signature
PierceHolesList()
Returns: Return type: NXOpen.Die.PierceItemBuilderList
New in version NX5.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
PrecisionType¶
-
PierceTaskBuilder.
PrecisionType
¶ Returns or sets the precision type of the pierce task
-------------------------------------
Getter Method
Signature
PrecisionType()
Returns: Return type: NXOpen.Die.PierceTaskBuilderPrecisionTypes
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
PrecisionType(precisionType)
Parameters: precisionType ( NXOpen.Die.PierceTaskBuilderPrecisionTypes
) –New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
TipFeature¶
-
PierceTaskBuilder.
TipFeature
¶ Returns the tip feature
-------------------------------------
Getter Method
Signature
TipFeature()
Returns: Return type: NXOpen.Features.SelectFeature
New in version NX5.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
TippedProduct¶
-
PierceTaskBuilder.
TippedProduct
¶ Returns or sets the tipped product of the pierce task
-------------------------------------
Getter Method
Signature
TippedProduct()
Returns: The tip of the operation where the pierce task resides. :rtype:
NXOpen.Features.Feature
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
TippedProduct(tippedProduct)
Parameters: tippedProduct ( NXOpen.Features.Feature
) – The tip of the operation where the pierce task resides.New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
TrimNewDieFace¶
-
PierceTaskBuilder.
TrimNewDieFace
¶ Returns or sets the trim new die face, from NX10.
0 new stamping output can import one new die face to die engineer process. If this pierce task will trim this new die face, set trimNewDieFace to true, or else set it to false.
-------------------------------------
Getter Method
Signature
TrimNewDieFace()
Returns: if pierce task performs on new die face, this will be true, or else this will be false. Return type: bool New in version NX10.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
TrimNewDieFace(trimNewDieFace)
Parameters: trimNewDieFace (bool) – if set to true, pierce task performs on new die face, or else it will perform on original die face. New in version NX10.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
WithoutWorkflowSheet¶
-
PierceTaskBuilder.
WithoutWorkflowSheet
¶ Returns or sets the without workflow sheet of the pierce task builder.
In release NX11.0, pierce task supports without workflow type when the workflow tip feature does not exist.
-------------------------------------
Getter Method
Signature
WithoutWorkflowSheet()
Returns: Return type: NXOpen.Body
New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
WithoutWorkflowSheet(sheet)
Parameters: sheet ( NXOpen.Body
) –New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
Method Detail¶
GetAssociativeObjects¶
-
PierceTaskBuilder.
GetAssociativeObjects
¶ Gets the associative objects of the pierce task
Signature
GetAssociativeObjects()
Returns: Return type: list of NXOpen.DisplayableObject
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
GetCameraLayerAndXmlp¶
-
PierceTaskBuilder.
GetCameraLayerAndXmlp
¶ Gets the camera layer settings and xmlp data
Signature
GetCameraLayerAndXmlp()
Returns: a tuple Return type: A tuple consisting of (layerSettings, xmlpData). layerSettings is a list of str. 1 layer setting string for each camera object. the string needs to be 256 characters long (one for each user layer) with either 0 for off or 1 for on. xmlpData is a list of str. xmlp data New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
GetCameraNames¶
-
PierceTaskBuilder.
GetCameraNames
¶ Gets the names of the camera
Signature
GetCameraNames()
Returns: each string contains the name of a camera object Return type: list of str New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
GetCameraViews¶
-
PierceTaskBuilder.
GetCameraViews
¶ Gets the camera views of the pierce task
Signature
GetCameraViews()
Returns: Return type: list of NXOpen.View
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
GetDetails¶
-
PierceTaskBuilder.
GetDetails
¶ Gets the detailed description of the pierce task
Signature
GetDetails()
Returns: detail strings Return type: list of str New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
GetPierceBounds¶
-
PierceTaskBuilder.
GetPierceBounds
¶ Gets the pierce bounds of the pierce task
Signature
GetPierceBounds()
Returns: a tuple Return type: A tuple consisting of (profileEntries, direction). profileEntries is a list of NXOpen.IProfile
. Profile entries that make up the boundary of the pierce task direction is aNXOpen.Die.DirectionOption
. Profile directionNew in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
NewPierceHole¶
-
PierceTaskBuilder.
NewPierceHole
¶ Creates a new pierce hole item in the set
Signature
NewPierceHole(holeShape)
Parameters: holeShape ( NXOpen.Die.PierceItemBuilderHoleShapeType
) –Returns: Return type: NXOpen.Die.PierceItemBuilder
New in version NX5.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SetAssociativeObjects¶
-
PierceTaskBuilder.
SetAssociativeObjects
¶ Sets the associative objects of the pierce task
Signature
SetAssociativeObjects(objects)
Parameters: objects (list of NXOpen.DisplayableObject
) –New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SetCameraLayerAndXmlp¶
-
PierceTaskBuilder.
SetCameraLayerAndXmlp
¶ Sets the camera layer settings and xmlp data
Signature
SetCameraLayerAndXmlp(layerSettings, xmlpData)
Parameters: - layerSettings (list of str) – 1 layer setting string for each camera object. the string needs to be 256 characters long (one for each user layer) with either 0 for off or 1 for on.
- xmlpData (list of str) – xmlp data
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SetCameraNames¶
-
PierceTaskBuilder.
SetCameraNames
¶ Sets the names of the camera
Signature
SetCameraNames(strings)
Parameters: strings (list of str) – each string contains the name of a camera object New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SetCameraViews¶
-
PierceTaskBuilder.
SetCameraViews
¶ Sets the camera views of the pierce task
Signature
SetCameraViews(objects)
Parameters: objects (list of NXOpen.View
) –New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SetDetails¶
-
PierceTaskBuilder.
SetDetails
¶ Sets the detailed description of the pierce task
Signature
SetDetails(strings)
Parameters: strings (list of str) – detail strings New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SetPierceBounds¶
-
PierceTaskBuilder.
SetPierceBounds
¶ Sets the pierce bounds of the pierce task.
Note -
Die.PierceTaskBuilder.TippedProduct()
needs to be called before this function.Signature
SetPierceBounds(direction, profileEntries)
Parameters: - direction (
NXOpen.Die.DirectionOption
) – Profile direction - profileEntries (list of
NXOpen.IProfile
) – Profile entries that make up the boundary of the pierce task
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
- direction (
Validate¶
-
PierceTaskBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.