PierceTaskBuilderCamTypes Enumeration

NXOpen.Die.PierceTaskBuilder.CamTypes is an alias for NXOpen.Die.PierceTaskBuilderCamTypes

class NXOpen.Die.PierceTaskBuilderCamTypes

Bases: object

Settings for the cam type of the pierce task.

Enum Members

Enum Member Enum Member Description
Direct
Direct
Aerial
Aerial Cam
BaseMounted
Base Mounted Cam
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.