DirectionOption Enumeration

class NXOpen.Die.DirectionOption

Bases: object

Settings for the profile direction.

Enum Members

Enum Member Enum Member Description
FromEnd
Profile direction is aligned with the first curve from the end to start.
FromStart
Profile direction is aligned with the first curve from the start to end.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.