PierceItemBuilderHoleShapeType Enumeration

NXOpen.Die.PierceItemBuilder.HoleShapeType is an alias for NXOpen.Die.PierceItemBuilderHoleShapeType

class NXOpen.Die.PierceItemBuilderHoleShapeType

Bases: object

Settings for the hole shape of individual pierces.

Enum Members

Enum Member Enum Member Description
Circular
Circular shaped hole
Oblong
Oblong shaped hole
Square
Square shaped hole
Rectangular
Rectangular shaped hole
RoundedRectangular
Rouned Rectangular shaped hole
ChordRectangular
Chord Rectangular hole
Hexagonal
Hexagonal shaped hole
Other
Not a standard shape
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.