MachineReliefBuilder Class¶
-
class
NXOpen.Die.
MachineReliefBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a builder that is used to create or edit a
NXOpen.Die.MachineRelief
feature.The builder may generate a Cam Definition, Machine Relief, or Wall Thickness.
To create a new instance of this class, use
NXOpen.Die.DieCollection.CreateMachineReliefBuilder()
Default values.
Property Value BaseOffset.Value 0 (millimeters part), 0 (inches part) BeltFaceThickness.Value 20 (millimeters part), 0.8 (inches part) End.InputType SelectLocation JogWall 0 MainProfileType Exterior Offset.Value 20 (millimeters part), 0.8 (inches part) ProfileOffset.Value 30 (millimeters part), 1.2 (inches part) Relief.Value 20 (millimeters part), 0.8 (inches part) ReliefOffset.Value 5 (millimeters part), 0.2 (inches part) TopOffset.Value 1000 (millimeters part), 40 (inches part) TrimOffset.Value 5 (millimeters part), 0.2 (inches part) TrimSheetOffset.Value 0 (millimeters part), 0 (inches part) TrimSheetType Sheet WallOffset.Value 10 (millimeters part), 0.4 (inches part) WallThickness.Value 45 (millimeters part), 1.8 (inches part) New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the angle tolerance. |
BaseOffset | Returns the expression containing the offset value to apply to the base definition before trimming the base of the tool solids. |
BaseOrientation | Returns the base orientation of the target solid. |
BeltAttributes | Returns the attribute title, value and face color to apply to the belt faces. |
BeltFaceThickness | Returns the expression containing the value to apply for the belt face on the cam definition. |
CamDirection | Returns the direction of the cam for trimming. |
DistanceTolerance | Returns or sets the distance tolerance. |
End | Returns the location for the end of the segment definition. |
InsideWallProfile | Returns the wall profile defining the inside of the main wall used for the cam definition. |
JogWall | Returns or sets the indicator defining if the wall should be jogged (or changed) to accommodate the cam definition. |
MainProfile | Returns the primary profile for the machine relief casting. |
MainProfileType | Returns or sets the value specifying the main profile for the Thicken operation. |
Offset | Returns the expression containing the value to apply for the thicken operation to create the tool solid. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ProfileOffset | Returns the expression containing the value to apply to the profile to create the primary head solid for the cam definition. |
Relief | Returns the expression containing the value to apply for the machine relief operation to create the tool solid. |
ReliefOffset | Returns the expression containing the value of the relief around the primary head solid for the cam definition if a wall is created. |
Start | Returns the location for the start of the segment definition. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
SwitchTrimSide | Returns or sets the indicator if the trim side should be switched from the default for the sheet metal. |
Tag | Returns the Tag for this object. |
Target | Returns the target solid to add or subtract material too. |
TopOffset | Returns the expression containing the offset value from the base to define the top extent of the internal builds. |
TrimOffset | Returns the expression containing the clearance value to apply at the start and the end of the cam definition to define the primary head solid. |
TrimSheet | Returns the sheet body selection for the trim sheet. |
TrimSheetFace | Returns the face selections to define the trim sheet. |
TrimSheetOffset | Returns the expression containing the offset value to apply to the trim sheet to construct the tool solids. |
TrimSheetType | Returns or sets the indicator for how the trim sheet is specified. |
Type | Returns or sets the value defining the type of build to perform for this tool. |
WallOffset | Returns the expression containing the offset to apply to the wall to create the wall area for the cam definition. |
WallThickness | Returns the expression containing the thickness value of the wall for the cam definition. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MachineReliefBuilderMainProfileTypes Enumeration | Specifies that the profile is for an exterior or interior profile. |
MachineReliefBuilderTrimSheetTypes Enumeration | Specifies what the trimming surface is defined by. |
MachineReliefBuilderTypes Enumeration | Identifies the type of structure to be added, or subtracted, to the casting. |
Property Detail¶
AngleTolerance¶
-
MachineReliefBuilder.
AngleTolerance
¶ Returns or sets the angle tolerance.
-------------------------------------
Getter Method
Signature
AngleTolerance()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleTolerance(angleTolerance)
Parameters: angleTolerance (float) – New in version NX7.5.0.
License requirements: ug_die_design (“Die Design”)
BaseOffset¶
-
MachineReliefBuilder.
BaseOffset
¶ Returns the expression containing the offset value to apply to the base definition before trimming the base of the tool solids.
-------------------------------------
Getter Method
Signature
BaseOffset()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
BaseOrientation¶
-
MachineReliefBuilder.
BaseOrientation
¶ Returns the base orientation of the target solid.
-------------------------------------
Getter Method
Signature
BaseOrientation()
Returns: Return type: NXOpen.Die.DiePlaneBuilder
New in version NX7.5.0.
License requirements: None.
BeltAttributes¶
-
MachineReliefBuilder.
BeltAttributes
¶ Returns the attribute title, value and face color to apply to the belt faces.
-------------------------------------
Getter Method
Signature
BeltAttributes()
Returns: Return type: NXOpen.Die.DieAttributesBuilder
New in version NX7.5.0.
License requirements: None.
BeltFaceThickness¶
-
MachineReliefBuilder.
BeltFaceThickness
¶ Returns the expression containing the value to apply for the belt face on the cam definition.
Only valid when type is
Die.MachineReliefBuilderTypes.Cam
.-------------------------------------
Getter Method
Signature
BeltFaceThickness()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
CamDirection¶
-
MachineReliefBuilder.
CamDirection
¶ Returns the direction of the cam for trimming.
Only valid when type is
Die.MachineReliefBuilderTypes.Cam
orDie.MachineReliefBuilderTypes.Relief
.-------------------------------------
Getter Method
Signature
CamDirection()
Returns: Return type: NXOpen.Die.DieDirectionBuilder
New in version NX7.5.0.
License requirements: None.
DistanceTolerance¶
-
MachineReliefBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance.
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX7.5.0.
License requirements: ug_die_design (“Die Design”)
End¶
-
MachineReliefBuilder.
End
¶ Returns the location for the end of the segment definition.
The default is the end of the segment if an open profile is selected.
-------------------------------------
Getter Method
Signature
End()
Returns: Return type: NXOpen.Die.DieLocationBuilder
New in version NX7.5.0.
License requirements: None.
InsideWallProfile¶
-
MachineReliefBuilder.
InsideWallProfile
¶ Returns the wall profile defining the inside of the main wall used for the cam definition.
Only valid when type is
Die.MachineReliefBuilderTypes.Cam
.-------------------------------------
Getter Method
Signature
InsideWallProfile()
Returns: Return type: NXOpen.Section
New in version NX7.5.0.
License requirements: None.
JogWall¶
-
MachineReliefBuilder.
JogWall
¶ Returns or sets the indicator defining if the wall should be jogged (or changed) to accommodate the cam definition.
TRUE indicates that the wal should be jogged.
-------------------------------------
Getter Method
Signature
JogWall()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
JogWall(jogWall)
Parameters: jogWall (bool) – New in version NX7.5.0.
License requirements: ug_die_design (“Die Design”)
MainProfile¶
-
MachineReliefBuilder.
MainProfile
¶ Returns the primary profile for the machine relief casting.
-------------------------------------
Getter Method
Signature
MainProfile()
Returns: Return type: NXOpen.Section
New in version NX7.5.0.
License requirements: None.
MainProfileType¶
-
MachineReliefBuilder.
MainProfileType
¶ Returns or sets the value specifying the main profile for the Thicken operation.
Only valid when type is
Die.MachineReliefBuilderTypes.Thicken
.-------------------------------------
Getter Method
Signature
MainProfileType()
Returns: Return type: NXOpen.Die.MachineReliefBuilderMainProfileTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MainProfileType(mainProfileType)
Parameters: mainProfileType ( NXOpen.Die.MachineReliefBuilderMainProfileTypes
) –New in version NX7.5.0.
License requirements: ug_die_design (“Die Design”)
Offset¶
-
MachineReliefBuilder.
Offset
¶ Returns the expression containing the value to apply for the thicken operation to create the tool solid.
Only valid when type is
Die.MachineReliefBuilderTypes.Relief
orDie.MachineReliefBuilderTypes.Thicken
.-------------------------------------
Getter Method
Signature
Offset()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
ProfileOffset¶
-
MachineReliefBuilder.
ProfileOffset
¶ Returns the expression containing the value to apply to the profile to create the primary head solid for the cam definition.
Only valid when type is
Die.MachineReliefBuilderTypes.Cam
.-------------------------------------
Getter Method
Signature
ProfileOffset()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
Relief¶
-
MachineReliefBuilder.
Relief
¶ Returns the expression containing the value to apply for the machine relief operation to create the tool solid.
Only valid when type is
Die.MachineReliefBuilderTypes.Relief
orDie.MachineReliefBuilderTypes.Thicken
.-------------------------------------
Getter Method
Signature
Relief()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
ReliefOffset¶
-
MachineReliefBuilder.
ReliefOffset
¶ Returns the expression containing the value of the relief around the primary head solid for the cam definition if a wall is created.
Only valid when type is
Die.MachineReliefBuilderTypes.Cam
.-------------------------------------
Getter Method
Signature
ReliefOffset()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
Start¶
-
MachineReliefBuilder.
Start
¶ Returns the location for the start of the segment definition.
The default is the start of the segment if an open profile is selected.
-------------------------------------
Getter Method
Signature
Start()
Returns: Return type: NXOpen.Die.DieLocationBuilder
New in version NX7.5.0.
License requirements: None.
SwitchTrimSide¶
-
MachineReliefBuilder.
SwitchTrimSide
¶ Returns or sets the indicator if the trim side should be switched from the default for the sheet metal.
TRUE indicates that the trim side should be reversed.
-------------------------------------
Getter Method
Signature
SwitchTrimSide()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SwitchTrimSide(switchTrimSide)
Parameters: switchTrimSide (bool) – New in version NX7.5.0.
License requirements: ug_die_design (“Die Design”)
Target¶
-
MachineReliefBuilder.
Target
¶ Returns the target solid to add or subtract material too.
-------------------------------------
Getter Method
Signature
Target()
Returns: Return type: NXOpen.SelectBody
New in version NX7.5.0.
License requirements: None.
TopOffset¶
-
MachineReliefBuilder.
TopOffset
¶ Returns the expression containing the offset value from the base to define the top extent of the internal builds.
This value will be defined internally if a target is selected.
-------------------------------------
Getter Method
Signature
TopOffset()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
TrimOffset¶
-
MachineReliefBuilder.
TrimOffset
¶ Returns the expression containing the clearance value to apply at the start and the end of the cam definition to define the primary head solid.
Only valid when type is
Die.MachineReliefBuilderTypes.Cam
.-------------------------------------
Getter Method
Signature
TrimOffset()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
TrimSheet¶
-
MachineReliefBuilder.
TrimSheet
¶ Returns the sheet body selection for the trim sheet.
-------------------------------------
Getter Method
Signature
TrimSheet()
Returns: Return type: NXOpen.SelectBody
New in version NX7.5.0.
License requirements: None.
TrimSheetFace¶
-
MachineReliefBuilder.
TrimSheetFace
¶ Returns the face selections to define the trim sheet.
-------------------------------------
Getter Method
Signature
TrimSheetFace()
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
TrimSheetOffset¶
-
MachineReliefBuilder.
TrimSheetOffset
¶ Returns the expression containing the offset value to apply to the trim sheet to construct the tool solids.
Only valid when type is
Die.MachineReliefBuilderTypes.Relief
orDie.MachineReliefBuilderTypes.Thicken
.-------------------------------------
Getter Method
Signature
TrimSheetOffset()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
TrimSheetType¶
-
MachineReliefBuilder.
TrimSheetType
¶ Returns or sets the indicator for how the trim sheet is specified.
-------------------------------------
Getter Method
Signature
TrimSheetType()
Returns: Return type: NXOpen.Die.MachineReliefBuilderTrimSheetTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TrimSheetType(trimSheetType)
Parameters: trimSheetType ( NXOpen.Die.MachineReliefBuilderTrimSheetTypes
) –New in version NX7.5.0.
License requirements: ug_die_design (“Die Design”)
Type¶
-
MachineReliefBuilder.
Type
¶ Returns or sets the value defining the type of build to perform for this tool.
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Die.MachineReliefBuilderTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Die.MachineReliefBuilderTypes
) –New in version NX7.5.0.
License requirements: ug_die_design (“Die Design”)
WallOffset¶
-
MachineReliefBuilder.
WallOffset
¶ Returns the expression containing the offset to apply to the wall to create the wall area for the cam definition.
Only valid when type is
Die.MachineReliefBuilderTypes.Cam
.-------------------------------------
Getter Method
Signature
WallOffset()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
WallThickness¶
-
MachineReliefBuilder.
WallThickness
¶ Returns the expression containing the thickness value of the wall for the cam definition.
Only valid when type is
Die.MachineReliefBuilderTypes.Cam
.-------------------------------------
Getter Method
Signature
WallThickness()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
MachineReliefBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.