DieAttributesBuilder Class¶
-
class
NXOpen.Die.
DieAttributesBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Die.DieAttributesBuilder
.The Die Attributes class is a helper to the main Die Design feature to gather the attribute title and value and face color to be applied. The attribute will be applied to a face or faces in the application of varying types, such as a base face.
To create a new instance of this class, use
NXOpen.Die.DieCollection.CreateDieAttribute()
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AttributeColor | Returns or sets the color to be applied to the face, or faces, in the application |
AttributeTitle | Returns or sets the title of the attribute to be applied |
AttributeValue | Returns or sets the value given to the attribute |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AttributeColor¶
-
DieAttributesBuilder.
AttributeColor
¶ Returns or sets the color to be applied to the face, or faces, in the application
-------------------------------------
Getter Method
Signature
AttributeColor()
Returns: Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AttributeColor(attributeColor)
Parameters: attributeColor (Id) – New in version NX6.0.0.
License requirements: None.
AttributeTitle¶
-
DieAttributesBuilder.
AttributeTitle
¶ Returns or sets the title of the attribute to be applied
-------------------------------------
Getter Method
Signature
AttributeTitle()
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AttributeTitle(attributeTitle)
Parameters: attributeTitle (str) – New in version NX6.0.0.
License requirements: None.
AttributeValue¶
-
DieAttributesBuilder.
AttributeValue
¶ Returns or sets the value given to the attribute
-------------------------------------
Getter Method
Signature
AttributeValue()
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AttributeValue(attributeValue)
Parameters: attributeValue (str) – New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
DieAttributesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.