MachineReliefBuilderMainProfileTypes Enumeration¶
NXOpen.Die.MachineReliefBuilder.MainProfileTypes is an alias for NXOpen.Die.MachineReliefBuilderMainProfileTypes
-
class
NXOpen.Die.
MachineReliefBuilderMainProfileTypes
¶ Bases:
object
Specifies that the profile is for an exterior or interior profile.
This is necessary when the target supplies the profile
Enum Members
Enum Member Enum Member Description Exterior Profile is for the exterior surface of the main wall.Interior Profile is for the interior surface of the main wall.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-