KeywayBuilder Class¶
-
class
NXOpen.Die.
KeywayBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Die.KeywayBuilder
builderTo create a new instance of this class, use
NXOpen.Die.DieCollection.Keyway()
Default values.
Property Value AngleTolerance 0.5 CreateWithPad 1 DeckThickness.Value 0 (millimeters part), 0 (inches part) DistanceTolerance 0.0254 (millimeters part), 0.001 (inches part) Location PositiveX MinimumRibHeight.Value 200 (millimeters part), 8 (inches part) Offset.Value 0 (millimeters part), 0 (inches part) PadHeight.Value 65 (millimeters part), 2.6 (inches part) PadWidth.Value 60 (millimeters part), 2.4 (inches part) PlacementOffset.Value 0 (millimeters part), 0 (inches part) RunoffDepth.Value 40 (millimeters part), 1.6 (inches part) RunoffLength.Value 60 (millimeters part), 2.4 (inches part) RunoffRadius.Value 30 (millimeters part), 1.2 (inches part) RunoffWidth.Value 16 (millimeters part), 0.625 (inches part) SlotDepth.Value 20 (millimeters part), 0.8 (inches part) SlotLength.Value 100 (millimeters part), 4 (inches part) SlotWidth.Value 25 (millimeters part), 1 (inches part) New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the angle tolerance |
BaseFlange | Returns the closed loop section representing the base flange |
BaseOrientation | Returns the bottom orientation plane of the keyway pad |
CreateWithPad | Returns or sets the value, true or false) to decide if the pad should be created for the keyway |
DeckThickness | Returns the expression for the deck thickness |
DieCenterlineCoordinateSystem | Returns the die centerline coordinate system for orienting the keyway |
DistanceTolerance | Returns or sets the distance tolerance |
InteriorProfile | Returns the closed loop section representing the interior profile of the casting |
Location | Returns or sets the location for the keyway |
MinimumRibHeight | Returns the expression for the minimum rib height |
Offset | Returns the amount to offset the keyway perpendicular to the slot orientation |
PadAttributes | Returns the pad attributes |
PadHeight | Returns the expression for the pad height |
PadWidth | Returns the expression for the pad width |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PlacementOffset | Returns the amount to offset the base orientation |
RunoffDepth | Returns the expression for the runoff depth |
RunoffLength | Returns the expression for the runoff length |
RunoffRadius | Returns the expression for the runoff radius |
RunoffWidth | Returns the expression for the runoff width |
SheetMetal | Returns the sheet metal being formed by the casting. |
SlotAttributes | Returns the slot attributes |
SlotDepth | Returns the expression for the slot depth |
SlotLength | Returns the expression for the slot length |
SlotWidth | Returns the expression for the slot width |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Target | Returns the target solid the keyway will be united with |
Type | Returns or sets the type of the keyway runoff |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
KeywayBuilderLocationType Enumeration | Keyway location direction relative to the die centerline coordinate system |
KeywayBuilderTypes Enumeration | Keyway runoff types |
Property Detail¶
AngleTolerance¶
-
KeywayBuilder.
AngleTolerance
¶ Returns or sets the angle tolerance
-------------------------------------
Getter Method
Signature
AngleTolerance()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleTolerance(angleTolerance)
Parameters: angleTolerance (float) – New in version NX6.0.0.
License requirements: ug_die_design (“Die Design”)
BaseFlange¶
-
KeywayBuilder.
BaseFlange
¶ Returns the closed loop section representing the base flange
-------------------------------------
Getter Method
Signature
BaseFlange()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
BaseOrientation¶
-
KeywayBuilder.
BaseOrientation
¶ Returns the bottom orientation plane of the keyway pad
-------------------------------------
Getter Method
Signature
BaseOrientation()
Returns: Return type: NXOpen.Die.DiePlaneBuilder
New in version NX6.0.0.
License requirements: None.
CreateWithPad¶
-
KeywayBuilder.
CreateWithPad
¶ Returns or sets the value, true or false) to decide if the pad should be created for the keyway
-------------------------------------
Getter Method
Signature
CreateWithPad()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CreateWithPad(createWithPad)
Parameters: createWithPad (bool) – New in version NX6.0.0.
License requirements: ug_die_design (“Die Design”)
DeckThickness¶
-
KeywayBuilder.
DeckThickness
¶ Returns the expression for the deck thickness
-------------------------------------
Getter Method
Signature
DeckThickness()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
DieCenterlineCoordinateSystem¶
-
KeywayBuilder.
DieCenterlineCoordinateSystem
¶ Returns the die centerline coordinate system for orienting the keyway
-------------------------------------
Getter Method
Signature
DieCenterlineCoordinateSystem()
Returns: Return type: NXOpen.SelectCartesianCoordinateSystem
New in version NX6.0.0.
License requirements: None.
DistanceTolerance¶
-
KeywayBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX6.0.0.
License requirements: ug_die_design (“Die Design”)
InteriorProfile¶
-
KeywayBuilder.
InteriorProfile
¶ Returns the closed loop section representing the interior profile of the casting
-------------------------------------
Getter Method
Signature
InteriorProfile()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
Location¶
-
KeywayBuilder.
Location
¶ Returns or sets the location for the keyway
-------------------------------------
Getter Method
Signature
Location()
Returns: Return type: NXOpen.Die.KeywayBuilderLocationType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Location(location)
Parameters: location ( NXOpen.Die.KeywayBuilderLocationType
) –New in version NX6.0.0.
License requirements: ug_die_design (“Die Design”)
MinimumRibHeight¶
-
KeywayBuilder.
MinimumRibHeight
¶ Returns the expression for the minimum rib height
-------------------------------------
Getter Method
Signature
MinimumRibHeight()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
Offset¶
-
KeywayBuilder.
Offset
¶ Returns the amount to offset the keyway perpendicular to the slot orientation
-------------------------------------
Getter Method
Signature
Offset()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
PadAttributes¶
-
KeywayBuilder.
PadAttributes
¶ Returns the pad attributes
-------------------------------------
Getter Method
Signature
PadAttributes()
Returns: Return type: NXOpen.Die.DieAttributesBuilder
New in version NX6.0.0.
License requirements: None.
PadHeight¶
-
KeywayBuilder.
PadHeight
¶ Returns the expression for the pad height
-------------------------------------
Getter Method
Signature
PadHeight()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
PadWidth¶
-
KeywayBuilder.
PadWidth
¶ Returns the expression for the pad width
-------------------------------------
Getter Method
Signature
PadWidth()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
PlacementOffset¶
-
KeywayBuilder.
PlacementOffset
¶ Returns the amount to offset the base orientation
-------------------------------------
Getter Method
Signature
PlacementOffset()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
RunoffDepth¶
-
KeywayBuilder.
RunoffDepth
¶ Returns the expression for the runoff depth
-------------------------------------
Getter Method
Signature
RunoffDepth()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
RunoffLength¶
-
KeywayBuilder.
RunoffLength
¶ Returns the expression for the runoff length
-------------------------------------
Getter Method
Signature
RunoffLength()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
RunoffRadius¶
-
KeywayBuilder.
RunoffRadius
¶ Returns the expression for the runoff radius
-------------------------------------
Getter Method
Signature
RunoffRadius()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
RunoffWidth¶
-
KeywayBuilder.
RunoffWidth
¶ Returns the expression for the runoff width
-------------------------------------
Getter Method
Signature
RunoffWidth()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
SheetMetal¶
-
KeywayBuilder.
SheetMetal
¶ Returns the sheet metal being formed by the casting.
Used to measure the height.
-------------------------------------
Getter Method
Signature
SheetMetal()
Returns: Return type: NXOpen.SelectNXObject
New in version NX6.0.0.
License requirements: None.
SlotAttributes¶
-
KeywayBuilder.
SlotAttributes
¶ Returns the slot attributes
-------------------------------------
Getter Method
Signature
SlotAttributes()
Returns: Return type: NXOpen.Die.DieAttributesBuilder
New in version NX6.0.0.
License requirements: None.
SlotDepth¶
-
KeywayBuilder.
SlotDepth
¶ Returns the expression for the slot depth
-------------------------------------
Getter Method
Signature
SlotDepth()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
SlotLength¶
-
KeywayBuilder.
SlotLength
¶ Returns the expression for the slot length
-------------------------------------
Getter Method
Signature
SlotLength()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
SlotWidth¶
-
KeywayBuilder.
SlotWidth
¶ Returns the expression for the slot width
-------------------------------------
Getter Method
Signature
SlotWidth()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
Target¶
-
KeywayBuilder.
Target
¶ Returns the target solid the keyway will be united with
-------------------------------------
Getter Method
Signature
Target()
Returns: Return type: NXOpen.SelectNXObject
New in version NX6.0.0.
License requirements: None.
Type¶
-
KeywayBuilder.
Type
¶ Returns or sets the type of the keyway runoff
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Die.KeywayBuilderTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Die.KeywayBuilderTypes
) –New in version NX6.0.0.
License requirements: ug_die_design (“Die Design”)
Method Detail¶
Validate¶
-
KeywayBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.