KeywayBuilderTypes Enumeration

NXOpen.Die.KeywayBuilder.Types is an alias for NXOpen.Die.KeywayBuilderTypes

class NXOpen.Die.KeywayBuilderTypes

Bases: object

Keyway runoff types

Enum Members

Enum Member Enum Member Description
Rectangular
tool runoff is perpendicular to slot
Circular
tool runoff is created using a plunge cut at the end of the slot
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.