NXOpen.Diagramming.Tables Package¶
Classes¶
CellBuilder Class | Represents a CellBuilder. |
CellRangeBuilder Class | Represents a CellRangeBuilder. |
CellSettingsBuilder Class | Represents a CellSettingsBuilder. |
ColumnBuilder Class | Represents a ColumnBuilder. |
ContinuationDataBuilder Class | Represents a ContinuationDataBuilder. |
RowBuilder Class | Represents a RowBuilder. |
Table Class | Represents the Table class. |
TableBuilder Class | Represents a TableBuilder. |
TableCollection Class | Represents a collection of Table. |
TableSettingsBuilder Class | Represents a TableSettingsBuilder. |
Enumerations¶
AnchorLocation Enumeration | Represents the table anchor location. |
ContentAlignment Enumeration | Represents the cell content alignment. |
ContinuationLocation Enumeration | Represents the table continuation location. |
HeaderLocation Enumeration | Represents the table header location. |
HeaderOrientation Enumeration | Represents the table header orientation. |
OverflowBehavior Enumeration | Represents the cell overflow behavior. |
SizingMethod Enumeration | Represents the column/row sizing method. |
ZeroDisplay Enumeration | Represents the cell zero display. |
Structs¶
SizedSymbol Struct | Represents sized symbol information. |