RowBuilder Class¶
-
class
NXOpen.Diagramming.Tables.
RowBuilder
¶ Bases:
NXOpen.Diagramming.Tables.CellRangeBuilder
Represents a RowBuilder.
This is a sub-builder class and cannot be directly instantiated
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
BottomBorder | Returns or sets the bottom border rendering properties. |
CanHide | Returns or sets the can hide flag. |
Hidden | Returns or sets the hidden flag. |
LeftBorder | Returns or sets the left border rendering properties. |
RightBorder | Returns or sets the right border rendering properties. |
Size | Returns or sets the size. |
SizingMethod | Returns or sets the sizing method. |
Tag | Returns the Tag for this object. |
TopBorder | Returns or sets the top border rendering properties. |
Methods¶
Method | Description |
---|---|
SetHeight | The method to set the height of a row. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
SetHeight¶
-
RowBuilder.
SetHeight
¶ The method to set the height of a row.
Signature
SetHeight(size)
Parameters: size (float) – New in version NX10.0.0.
License requirements: None.
Validate¶
-
RowBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.