TableBuilder Class¶
-
class
NXOpen.Diagramming.Tables.
TableBuilder
¶ Bases:
NXOpen.Diagramming.AnnotationBuilder
Represents a TableBuilder.
To create a new instance of this class, use
NXOpen.Diagramming.Tables.TableCollection.CreateTableBuilder()
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
BottomBorder | Returns the bottom border rendering properties. |
BoundaryDisplay | Returns or sets the visibility of boundary. |
BoundaryType | Returns or sets the boundary type of the annotation |
CellSettingsBuilder | Returns the default cell border settings. |
ContinuationDataBuilder | Returns the continuation data. |
FormattedStringBuilder | Returns the formatted string of the text. |
Height | Returns or sets the height. |
HeightPolicy | Returns or sets the height policy. |
Internal | Returns the flag that indicates if the sheet element is internal. |
Label | Returns the label of this sheet element. |
LabelName | Returns or sets the label name of this sheet element. |
LeftBorder | Returns the left border rendering properties. |
Location | Returns the location of the sheet element relative to another sheet element. |
LocationStyle | Returns or sets the location style. |
Locked | Returns or sets the locked flag. |
MirrorX | Returns or sets the sheet element to Mirror along the X axis. |
MirrorY | Returns or sets the sheet element to Mirror along the Y axis. |
NumberOfColumns | Returns or sets the number of columns. |
NumberOfHeaders | Returns or sets the number of headers. |
NumberOfRows | Returns or sets the number of rows. |
Owner | Returns or sets the owning sheet element. |
OwningSheet | Returns the owning sheet. |
ResizeOption | Returns or sets the resize option of the sheet element |
RightBorder | Returns the right border rendering properties. |
Rotation | Returns or sets the rotation angle that is counter clockwise and relative to the owner. |
SourceElement | Returns the source element that records which sheet element it is a copy of. |
TableSettingsBuilder | Returns the table settings. |
Tag | Returns the Tag for this object. |
Text | Returns or sets the text should be used only when textType is Diagramming. |
TextStyleBuilder | Returns the text style of the annotation. |
TextType | Returns or sets the text type. |
TopBorder | Returns the top border rendering properties. |
UpToDate | Returns the flag that indicates if the sheet element is up to date. |
Visible | Returns the flag that indicates if the sheet element is visible. |
Width | Returns or sets the width. |
WidthPolicy | Returns or sets the width policy. |
NXOpen.Diagramming.SheetElementBuilder.X | Returns or sets the absolute x coordinate. |
NXOpen.Diagramming.SheetElementBuilder.Y | Returns or sets the absolute y coordinate. |
ZDepth | Returns or sets the Z depth. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAllPorts | Gets all ports of this connectable element. |
GetAllowedTransformations | Get the allowed transformations of the sheet element. |
GetCell | The method to get the cell at the given row and column indexes. |
GetColumn | The method to get the column at the given column index. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFillColor | The method to get the fill color. |
GetHeader | The method to get the header at the given header index. |
GetHeaderCell | The method to get the header cell at the given row and column indexes. |
GetMinNodeSize | Gets the minimum node size values |
GetObject | Returns the object currently being edited by this builder. |
GetPorts | Gets ports of this connectable element by the direction. |
GetRow | The method to get the row at the given row index. |
InsertColumns | The method to insert the given number of columns after the given column index. |
InsertHeaders | The method to insert the given number of headers after the given header index. |
InsertRows | The method to insert the given number of rows after the given row index. |
MergeCells | The method to merge the cells in the given ranges. |
MergeHeaderCells | The method to merge the header cells in the given ranges. |
RemoveColumns | The method to remove the given number of columns starting with the given column index. |
RemoveHeaders | The method to remove the given number of headers starting with the given header index. |
RemoveRows | The method to remove the given number of rows starting with the given row index. |
SetFillColor | The method to set the fill color. |
SetMinNodeSize | Sets the minimum node size values |
SetOwningSheet | Set the owning sheet when the sheet element is created. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnMergeCell | The method to unmerge the cell at the given row and column indexes. |
UnMergeHeaderCell | The method to unmerge the header cell at the given row and column indexes. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BottomBorder¶
-
TableBuilder.
BottomBorder
¶ Returns the bottom border rendering properties.
-------------------------------------
Getter Method
Signature
BottomBorder()
Returns: Return type: NXOpen.Diagramming.RenderingPropertiesBuilder
New in version NX10.0.0.
License requirements: None.
CellSettingsBuilder¶
-
TableBuilder.
CellSettingsBuilder
¶ Returns the default cell border settings.
-------------------------------------
Getter Method
Signature
CellSettingsBuilder()
Returns: Return type: NXOpen.Diagramming.Tables.CellSettingsBuilder
New in version NX10.0.0.
License requirements: None.
ContinuationDataBuilder¶
-
TableBuilder.
ContinuationDataBuilder
¶ Returns the continuation data.
-------------------------------------
Getter Method
Signature
ContinuationDataBuilder()
Returns: Return type: NXOpen.Diagramming.Tables.ContinuationDataBuilder
New in version NX10.0.0.
License requirements: None.
LeftBorder¶
-
TableBuilder.
LeftBorder
¶ Returns the left border rendering properties.
-------------------------------------
Getter Method
Signature
LeftBorder()
Returns: Return type: NXOpen.Diagramming.RenderingPropertiesBuilder
New in version NX10.0.0.
License requirements: None.
Locked¶
-
TableBuilder.
Locked
¶ Returns or sets the locked flag.
-------------------------------------
Getter Method
Signature
Locked()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Locked(locked)
Parameters: locked (bool) – New in version NX10.0.0.
License requirements: None.
NumberOfColumns¶
-
TableBuilder.
NumberOfColumns
¶ Returns or sets the number of columns.
-------------------------------------
Getter Method
Signature
NumberOfColumns()
Returns: Return type: int New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberOfColumns(numColumns)
Parameters: numColumns (int) – New in version NX10.0.0.
License requirements: None.
NumberOfHeaders¶
-
TableBuilder.
NumberOfHeaders
¶ Returns or sets the number of headers.
-------------------------------------
Getter Method
Signature
NumberOfHeaders()
Returns: Return type: int New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberOfHeaders(numHeaders)
Parameters: numHeaders (int) – New in version NX10.0.0.
License requirements: None.
NumberOfRows¶
-
TableBuilder.
NumberOfRows
¶ Returns or sets the number of rows.
-------------------------------------
Getter Method
Signature
NumberOfRows()
Returns: Return type: int New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberOfRows(numRows)
Parameters: numRows (int) – New in version NX10.0.0.
License requirements: None.
RightBorder¶
-
TableBuilder.
RightBorder
¶ Returns the right border rendering properties.
-------------------------------------
Getter Method
Signature
RightBorder()
Returns: Return type: NXOpen.Diagramming.RenderingPropertiesBuilder
New in version NX10.0.0.
License requirements: None.
TableSettingsBuilder¶
-
TableBuilder.
TableSettingsBuilder
¶ Returns the table settings.
-------------------------------------
Getter Method
Signature
TableSettingsBuilder()
Returns: Return type: NXOpen.Diagramming.Tables.TableSettingsBuilder
New in version NX10.0.0.
License requirements: None.
TopBorder¶
-
TableBuilder.
TopBorder
¶ Returns the top border rendering properties.
-------------------------------------
Getter Method
Signature
TopBorder()
Returns: Return type: NXOpen.Diagramming.RenderingPropertiesBuilder
New in version NX10.0.0.
License requirements: None.
Method Detail¶
GetCell¶
-
TableBuilder.
GetCell
¶ The method to get the cell at the given row and column indexes.
Signature
GetCell(rowIndex, columnIndex)
Parameters: - rowIndex (int) –
- columnIndex (int) –
Returns: Return type: New in version NX10.0.0.
License requirements: None.
GetColumn¶
-
TableBuilder.
GetColumn
¶ The method to get the column at the given column index.
Signature
GetColumn(columnIndex)
Parameters: columnIndex (int) – Returns: Return type: NXOpen.Diagramming.Tables.ColumnBuilder
New in version NX10.0.0.
License requirements: None.
GetFillColor¶
-
TableBuilder.
GetFillColor
¶ The method to get the fill color.
Signature
GetFillColor()
Returns: a tuple Return type: A tuple consisting of (color, opacity). color is a Id. opacity is a float. New in version NX10.0.0.
License requirements: None.
GetHeader¶
-
TableBuilder.
GetHeader
¶ The method to get the header at the given header index.
Signature
GetHeader(headerIndex)
Parameters: headerIndex (int) – Returns: Return type: NXOpen.Diagramming.Tables.CellRangeBuilder
New in version NX10.0.0.
License requirements: None.
GetHeaderCell¶
-
TableBuilder.
GetHeaderCell
¶ The method to get the header cell at the given row and column indexes.
Signature
GetHeaderCell(rowIndex, columnIndex)
Parameters: - rowIndex (int) –
- columnIndex (int) –
Returns: Return type: New in version NX10.0.0.
License requirements: None.
GetRow¶
-
TableBuilder.
GetRow
¶ The method to get the row at the given row index.
Signature
GetRow(rowIndex)
Parameters: rowIndex (int) – Returns: Return type: NXOpen.Diagramming.Tables.RowBuilder
New in version NX10.0.0.
License requirements: None.
InsertColumns¶
-
TableBuilder.
InsertColumns
¶ The method to insert the given number of columns after the given column index.
Signature
InsertColumns(columnIndex, numColumns)
Parameters: - columnIndex (int) –
- numColumns (int) –
New in version NX10.0.0.
License requirements: None.
InsertHeaders¶
-
TableBuilder.
InsertHeaders
¶ The method to insert the given number of headers after the given header index.
Signature
InsertHeaders(headerIndex, numHeaders)
Parameters: - headerIndex (int) –
- numHeaders (int) –
New in version NX10.0.0.
License requirements: None.
InsertRows¶
-
TableBuilder.
InsertRows
¶ The method to insert the given number of rows after the given row index.
Signature
InsertRows(rowIndex, numRows)
Parameters: - rowIndex (int) –
- numRows (int) –
New in version NX10.0.0.
License requirements: None.
MergeCells¶
-
TableBuilder.
MergeCells
¶ The method to merge the cells in the given ranges.
Signature
MergeCells(topRow, leftColumn, bottomRow, rightColumn)
Parameters: - topRow (int) –
- leftColumn (int) –
- bottomRow (int) –
- rightColumn (int) –
New in version NX10.0.0.
License requirements: None.
MergeHeaderCells¶
-
TableBuilder.
MergeHeaderCells
¶ The method to merge the header cells in the given ranges.
Signature
MergeHeaderCells(topRow, leftColumn, bottomRow, rightColumn)
Parameters: - topRow (int) –
- leftColumn (int) –
- bottomRow (int) –
- rightColumn (int) –
New in version NX10.0.0.
License requirements: None.
RemoveColumns¶
-
TableBuilder.
RemoveColumns
¶ The method to remove the given number of columns starting with the given column index.
Signature
RemoveColumns(columnIndex, numColumns)
Parameters: - columnIndex (int) –
- numColumns (int) –
New in version NX10.0.0.
License requirements: None.
RemoveHeaders¶
-
TableBuilder.
RemoveHeaders
¶ The method to remove the given number of headers starting with the given header index.
Signature
RemoveHeaders(headerIndex, numHeaders)
Parameters: - headerIndex (int) –
- numHeaders (int) –
New in version NX10.0.0.
License requirements: None.
RemoveRows¶
-
TableBuilder.
RemoveRows
¶ The method to remove the given number of rows starting with the given row index.
Signature
RemoveRows(rowIndex, numRows)
Parameters: - rowIndex (int) –
- numRows (int) –
New in version NX10.0.0.
License requirements: None.
SetFillColor¶
UnMergeCell¶
-
TableBuilder.
UnMergeCell
¶ The method to unmerge the cell at the given row and column indexes.
Signature
UnMergeCell(rowIndex, columnIndex)
Parameters: - rowIndex (int) –
- columnIndex (int) –
New in version NX10.0.0.
License requirements: None.
UnMergeHeaderCell¶
-
TableBuilder.
UnMergeHeaderCell
¶ The method to unmerge the header cell at the given row and column indexes.
Signature
UnMergeHeaderCell(rowIndex, columnIndex)
Parameters: - rowIndex (int) –
- columnIndex (int) –
New in version NX10.0.0.
License requirements: None.
Validate¶
-
TableBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.