CellSettingsBuilder Class¶
-
class
NXOpen.Diagramming.Tables.
CellSettingsBuilder
¶ Bases:
NXOpen.Diagramming.BaseTaggedObjectBuilder
Represents a CellSettingsBuilder.
This is a sub-builder class and cannot be directly instantiated
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
BottomBorder | Returns the bottom border line rendering properties. |
ContentAlignment | Returns or sets the content alignment of the cell settings. |
FillColor | Returns or sets the fill color. |
FillOpacity | Returns or sets the fill opacity. |
OverflowBehavior | Returns or sets the overflow behavior of the cell settings. |
RightBorder | Returns the right border line rendering properties. |
Tag | Returns the Tag for this object. |
ZeroDisplay | Returns or sets the zero display of the cell settings. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BottomBorder¶
-
CellSettingsBuilder.
BottomBorder
¶ Returns the bottom border line rendering properties.
-------------------------------------
Getter Method
Signature
BottomBorder()
Returns: Return type: NXOpen.Diagramming.RenderingPropertiesBuilder
New in version NX10.0.0.
License requirements: None.
ContentAlignment¶
-
CellSettingsBuilder.
ContentAlignment
¶ Returns or sets the content alignment of the cell settings.
-------------------------------------
Getter Method
Signature
ContentAlignment()
Returns: Return type: NXOpen.Diagramming.Tables.ContentAlignment
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ContentAlignment(contentAlignment)
Parameters: contentAlignment ( NXOpen.Diagramming.Tables.ContentAlignment
) –New in version NX10.0.0.
License requirements: None.
FillColor¶
-
CellSettingsBuilder.
FillColor
¶ Returns or sets the fill color.
-------------------------------------
Getter Method
Signature
FillColor()
Returns: Return type: Id New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FillColor(colorId)
Parameters: colorId (Id) – New in version NX10.0.0.
License requirements: None.
FillOpacity¶
-
CellSettingsBuilder.
FillOpacity
¶ Returns or sets the fill opacity.
The range of opacity is from 0.0 to 1.0. 0.0 is completely transparent and 1.0 is completely opaque.
-------------------------------------
Getter Method
Signature
FillOpacity()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FillOpacity(opacity)
Parameters: opacity (float) – New in version NX10.0.0.
License requirements: None.
OverflowBehavior¶
-
CellSettingsBuilder.
OverflowBehavior
¶ Returns or sets the overflow behavior of the cell settings.
-------------------------------------
Getter Method
Signature
OverflowBehavior()
Returns: Return type: NXOpen.Diagramming.Tables.OverflowBehavior
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OverflowBehavior(overflowBehavior)
Parameters: overflowBehavior ( NXOpen.Diagramming.Tables.OverflowBehavior
) –New in version NX10.0.0.
License requirements: None.
RightBorder¶
-
CellSettingsBuilder.
RightBorder
¶ Returns the right border line rendering properties.
-------------------------------------
Getter Method
Signature
RightBorder()
Returns: Return type: NXOpen.Diagramming.RenderingPropertiesBuilder
New in version NX10.0.0.
License requirements: None.
ZeroDisplay¶
-
CellSettingsBuilder.
ZeroDisplay
¶ Returns or sets the zero display of the cell settings.
-------------------------------------
Getter Method
Signature
ZeroDisplay()
Returns: Return type: NXOpen.Diagramming.Tables.ZeroDisplay
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZeroDisplay(zeroDisplay)
Parameters: zeroDisplay ( NXOpen.Diagramming.Tables.ZeroDisplay
) –New in version NX10.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
CellSettingsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.