TeachmodeLinearMoveBuilder Class¶
-
class
NXOpen.CAM.
TeachmodeLinearMoveBuilder
¶ Bases:
NXOpen.CAM.MoveBuilder
Represents a TeachmodeLinearMove
To create a new instance of this class, use
NXOpen.CAM.OperationCollection.CreateTeachmodeTurningBuilder()
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
EndPositionType | Returns or sets the Type of End Position Definition |
FeedRate | Returns or sets the feed rate |
FeedType | Returns or sets the feed type |
FeedUnit | Returns or sets the feed unit |
FirstCurve | Returns or sets the First Curve |
FirstCurveStock | Returns or sets the Stock on first Curve |
FirstCurveToolPosition | Returns or sets the Tool Position to first Curve |
InitialRetractAngle | Returns or sets the initial retract angle |
InitialRetractDistance | Returns or sets the initial retract distance |
InitialRetractType | Returns or sets the Initial Retract Type |
MotionType | Returns or sets the motion type |
MoveType | Returns or sets the Movement Type |
NumberOfUserParameters | Returns the number of user parameters |
Point | Returns or sets the Point |
ProtectedMove | Returns or sets the protected move status |
SecondCurve | Returns or sets the Second Curve |
SecondCurveStock | Returns or sets the Stock on second Curve |
SecondCurveToolPosition | Returns or sets the Tool Position to second Curve |
SubopLabel | Returns or sets the subop label |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetUserParameter | Returns the custom parameter with the given name. |
SetParent | Set parent |
SetSibling | Set sibling |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
TeachmodeLinearMoveBuilderCurveToolPositionTypes Enumeration | the types for positioning to curves |
TeachmodeLinearMoveBuilderEndPositionTypes Enumeration | the end position definition types |
TeachmodeLinearMoveBuilderInitialRetractTypes Enumeration | the initial retract choices |
TeachmodeLinearMoveBuilderMoveTypes Enumeration | the movement types |
Property Detail¶
EndPositionType¶
-
TeachmodeLinearMoveBuilder.
EndPositionType
¶ Returns or sets the Type of End Position Definition
-------------------------------------
Getter Method
Signature
EndPositionType()
Returns: the end position type Return type: NXOpen.CAM.TeachmodeLinearMoveBuilderEndPositionTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndPositionType(newValue)
Parameters: newValue ( NXOpen.CAM.TeachmodeLinearMoveBuilderEndPositionTypes
) – the end position typeNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
FirstCurve¶
-
TeachmodeLinearMoveBuilder.
FirstCurve
¶ Returns or sets the First Curve
-------------------------------------
Getter Method
Signature
FirstCurve()
Returns: the first curve Return type: NXOpen.NXObject
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstCurve(newValue)
Parameters: newValue ( NXOpen.NXObject
) – the first curveNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
FirstCurveStock¶
-
TeachmodeLinearMoveBuilder.
FirstCurveStock
¶ Returns or sets the Stock on first Curve
-------------------------------------
Getter Method
Signature
FirstCurveStock()
Returns: the stock on first curve Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstCurveStock(newValue)
Parameters: newValue (float) – the stock on first curve New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
FirstCurveToolPosition¶
-
TeachmodeLinearMoveBuilder.
FirstCurveToolPosition
¶ Returns or sets the Tool Position to first Curve
-------------------------------------
Getter Method
Signature
FirstCurveToolPosition()
Returns: the tool position type Return type: NXOpen.CAM.TeachmodeLinearMoveBuilderCurveToolPositionTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstCurveToolPosition(newValue)
Parameters: newValue ( NXOpen.CAM.TeachmodeLinearMoveBuilderCurveToolPositionTypes
) – the tool position typeNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
InitialRetractAngle¶
-
TeachmodeLinearMoveBuilder.
InitialRetractAngle
¶ Returns or sets the initial retract angle
-------------------------------------
Getter Method
Signature
InitialRetractAngle()
Returns: the initial retract angle Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InitialRetractAngle(newValue)
Parameters: newValue (float) – the initial retract angle New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
InitialRetractDistance¶
-
TeachmodeLinearMoveBuilder.
InitialRetractDistance
¶ Returns or sets the initial retract distance
-------------------------------------
Getter Method
Signature
InitialRetractDistance()
Returns: the initial retract distance Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InitialRetractDistance(newValue)
Parameters: newValue (float) – the initial retract distance New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
InitialRetractType¶
-
TeachmodeLinearMoveBuilder.
InitialRetractType
¶ Returns or sets the Initial Retract Type
-------------------------------------
Getter Method
Signature
InitialRetractType()
Returns: the initial retract type Return type: NXOpen.CAM.TeachmodeLinearMoveBuilderInitialRetractTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InitialRetractType(newValue)
Parameters: newValue ( NXOpen.CAM.TeachmodeLinearMoveBuilderInitialRetractTypes
) – the initial retract typeNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
MoveType¶
-
TeachmodeLinearMoveBuilder.
MoveType
¶ Returns or sets the Movement Type
-------------------------------------
Getter Method
Signature
MoveType()
Returns: the move type Return type: NXOpen.CAM.TeachmodeLinearMoveBuilderMoveTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MoveType(newValue)
Parameters: newValue ( NXOpen.CAM.TeachmodeLinearMoveBuilderMoveTypes
) – the move typeNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
Point¶
-
TeachmodeLinearMoveBuilder.
Point
¶ Returns or sets the Point
-------------------------------------
Getter Method
Signature
Point()
Returns: the end point Return type: NXOpen.Point
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point(newValue)
Parameters: newValue ( NXOpen.Point
) – the pointNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
SecondCurve¶
-
TeachmodeLinearMoveBuilder.
SecondCurve
¶ Returns or sets the Second Curve
-------------------------------------
Getter Method
Signature
SecondCurve()
Returns: the second curve Return type: NXOpen.NXObject
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondCurve(newValue)
Parameters: newValue ( NXOpen.NXObject
) – the second curveNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
SecondCurveStock¶
-
TeachmodeLinearMoveBuilder.
SecondCurveStock
¶ Returns or sets the Stock on second Curve
-------------------------------------
Getter Method
Signature
SecondCurveStock()
Returns: the stock on second curve Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondCurveStock(newValue)
Parameters: newValue (float) – the stock on second curve New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
SecondCurveToolPosition¶
-
TeachmodeLinearMoveBuilder.
SecondCurveToolPosition
¶ Returns or sets the Tool Position to second Curve
-------------------------------------
Getter Method
Signature
SecondCurveToolPosition()
Returns: the tool position type Return type: NXOpen.CAM.TeachmodeLinearMoveBuilderCurveToolPositionTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondCurveToolPosition(newValue)
Parameters: newValue ( NXOpen.CAM.TeachmodeLinearMoveBuilderCurveToolPositionTypes
) – the tool position typeNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
TeachmodeLinearMoveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.