TeachmodeLinearMoveBuilderEndPositionTypes Enumeration

NXOpen.CAM.TeachmodeLinearMoveBuilder.EndPositionTypes is an alias for NXOpen.CAM.TeachmodeLinearMoveBuilderEndPositionTypes

class NXOpen.CAM.TeachmodeLinearMoveBuilderEndPositionTypes

Bases: object

the end position definition types

Enum Members

Enum Member Enum Member Description
Point
Point
Curves
Curves
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.