TeachmodeLinearMoveBuilderMoveTypes Enumeration

NXOpen.CAM.TeachmodeLinearMoveBuilder.MoveTypes is an alias for NXOpen.CAM.TeachmodeLinearMoveBuilderMoveTypes

class NXOpen.CAM.TeachmodeLinearMoveBuilderMoveTypes

Bases: object

the movement types

Enum Members

Enum Member Enum Member Description
Direct
Direct
Radial
Radial only
Axial
Axial only
RadialAxial
Radial then Axial
AxialRadial
Axial then Radial
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.