TeachmodeLinearMoveBuilderCurveToolPositionTypes Enumeration

NXOpen.CAM.TeachmodeLinearMoveBuilder.CurveToolPositionTypes is an alias for NXOpen.CAM.TeachmodeLinearMoveBuilderCurveToolPositionTypes

class NXOpen.CAM.TeachmodeLinearMoveBuilderCurveToolPositionTypes

Bases: object

the types for positioning to curves

Enum Members

Enum Member Enum Member Description
To
To Curve
On
On Curve
Past
Past Curve
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.