InspectionUVGridBuilder Class¶
-
class
NXOpen.CAM.
InspectionUVGridBuilder
¶ Bases:
NXOpen.CAM.InspectionMoveBuilder
Represents the builder for the CMM Inspection UV Grid sub-operation.
To create a new instance of this class, use
NXOpen.CAM.InspectionMoveCollection.CreateInspectionUvgridBuilder()
New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
AlignMachineAxes | Returns or sets the flag to align with machine axes |
AngleA | Returns or sets the A angle for an indexable head |
AngleB | Returns or sets the B angle for an indexable head |
ApproachDist | Returns the approach distance |
ApproachDistance | Returns or sets the approach distance |
DepthDistance | Returns or sets the depth distance |
DepthMethod | Returns or sets the depth method |
EndU | Returns the end value in U |
EndUDeg | Returns the end degrees value in U |
EndUDist | Returns the end distance value in U |
EndUMode | Returns or sets the end U mode |
EndUSweep | Returns the sweep value in U |
EndV | Returns the end value in V |
EndVDeg | Returns the end degrees value in V |
EndVDist | Returns the end distance value in V |
EndVMode | Returns or sets the end V mode |
EndVSweep | Returns the sweep value in V |
MeasuredGeometry | Returns or sets the measured geometry |
MotionType | Returns or sets the motion type |
NumberOfUPoints | Returns the number of points in U |
NumberOfVPoints | Returns the number of points in V |
NumberOfValidPoints | Returns or sets the number of valid points created for the UV Grid |
PointSequenceDirection | Returns or sets the point sequence start direction |
PointSequenceMode | Returns or sets the point sequence mode |
PointSequenceStart | Returns or sets the point sequence start location |
ProbeTipType | Returns or sets the preferred probe tip type |
ProbeTipTypeBuilder | Returns the Probe Tip Type Builder |
RetractDist | Returns the retract distance |
RetractDistance | Returns or sets the retract distance |
SearchDist | Returns the search distance |
SensorOpName | Returns or sets the inspection sensor operation name |
SensorStrategy | Returns or sets the sensor selection strategy |
SensorStrategyBuilder | Returns the Sensor Strategy Enum Builder |
SequenceOptimization | Returns or sets the path point sequence optimization setting |
SphereAxisMethod | Returns or sets the method for determining the axis for a sphere |
SphereAxisVector | Returns or sets the sphere axis vector |
StartPointMode | Returns or sets the start point mode |
StartU | Returns the start value in U |
StartUDeg | Returns the start degrees value in U |
StartUDist | Returns the start distance value in U |
StartUMode | Returns or sets the start U mode |
StartUSweep | Returns the start sweep value in U |
StartV | Returns the start value in V |
StartVDeg | Returns the start degrees value in V |
StartVDist | Returns the start distance value in V |
StartVMode | Returns or sets the start V mode |
StartVSweep | Returns the start sweep value in V |
Tag | Returns the Tag for this object. |
TipAngleMode | Returns or sets the tip angle selection mode |
TipMode | Returns or sets the probe tip selection mode |
TipNumber | Returns or sets the probe tip number |
UseFeatureCollisionAvoidance | Returns or sets the flag to use feature collision avoidance |
UsePartCollisionAvoidance | Returns or sets the flag to use part collision avoidance |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CopyAttributes | Copy point grid parameters |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetAppDistChanged | Flag indicating whether approach distance changed. |
SetLayoutChanged | Flag indicating whether layout changed. |
SetParent | Set parent |
SetPointCoverageChanged | Flag indicating whether point coverage changed. |
SetPointSequenceChanged | Flag indicating whether point sequence changed. |
SetProbeAngles | Set default values for probe angles based on feature type. |
SetProbeTip | Set default probe tip based on preferred tip type and probe angles. |
SetRetDistChanged | Flag indicating whether retract distance changed. |
SetSibling | Set sibling |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
InspectionUVGridBuilderSphereAxisType Enumeration | the method for determining the axis for a sphere |
InspectionUVGridBuilderStartPointType Enumeration | the start point mode |
Property Detail¶
AlignMachineAxes¶
-
InspectionUVGridBuilder.
AlignMachineAxes
¶ Returns or sets the flag to align with machine axes
-------------------------------------
Getter Method
Signature
AlignMachineAxes()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AlignMachineAxes(flag)
Parameters: flag (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ApproachDist¶
-
InspectionUVGridBuilder.
ApproachDist
¶ Returns the approach distance
-------------------------------------
Getter Method
Signature
ApproachDist()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.0.0.
License requirements: None.
DepthDistance¶
-
InspectionUVGridBuilder.
DepthDistance
¶ Returns or sets the depth distance
-------------------------------------
Getter Method
Signature
DepthDistance()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DepthDistance(distance)
Parameters: distance (float) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DepthMethod¶
-
InspectionUVGridBuilder.
DepthMethod
¶ Returns or sets the depth method
-------------------------------------
Getter Method
Signature
DepthMethod()
Returns: Return type: NXOpen.CAM.InspectionMoveBuilderDepthMethodTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DepthMethod(method)
Parameters: method ( NXOpen.CAM.InspectionMoveBuilderDepthMethodTypes
) –New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EndU¶
-
InspectionUVGridBuilder.
EndU
¶ Returns the end value in U
-------------------------------------
Getter Method
Signature
EndU()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.0.0.
License requirements: None.
EndUDeg¶
-
InspectionUVGridBuilder.
EndUDeg
¶ Returns the end degrees value in U
-------------------------------------
Getter Method
Signature
EndUDeg()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: None.
EndUDist¶
-
InspectionUVGridBuilder.
EndUDist
¶ Returns the end distance value in U
-------------------------------------
Getter Method
Signature
EndUDist()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: None.
EndUMode¶
-
InspectionUVGridBuilder.
EndUMode
¶ Returns or sets the end U mode
-------------------------------------
Getter Method
Signature
EndUMode()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderUVModeTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndUMode(uvMode)
Parameters: uvMode ( NXOpen.CAM.InspectionMethodBuilderUVModeTypes
) –New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EndUSweep¶
-
InspectionUVGridBuilder.
EndUSweep
¶ Returns the sweep value in U
-------------------------------------
Getter Method
Signature
EndUSweep()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: None.
EndV¶
-
InspectionUVGridBuilder.
EndV
¶ Returns the end value in V
-------------------------------------
Getter Method
Signature
EndV()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.0.0.
License requirements: None.
EndVDeg¶
-
InspectionUVGridBuilder.
EndVDeg
¶ Returns the end degrees value in V
-------------------------------------
Getter Method
Signature
EndVDeg()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: None.
EndVDist¶
-
InspectionUVGridBuilder.
EndVDist
¶ Returns the end distance value in V
-------------------------------------
Getter Method
Signature
EndVDist()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: None.
EndVMode¶
-
InspectionUVGridBuilder.
EndVMode
¶ Returns or sets the end V mode
-------------------------------------
Getter Method
Signature
EndVMode()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderUVModeTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndVMode(uvMode)
Parameters: uvMode ( NXOpen.CAM.InspectionMethodBuilderUVModeTypes
) –New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EndVSweep¶
-
InspectionUVGridBuilder.
EndVSweep
¶ Returns the sweep value in V
-------------------------------------
Getter Method
Signature
EndVSweep()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: None.
MeasuredGeometry¶
-
InspectionUVGridBuilder.
MeasuredGeometry
¶ Returns or sets the measured geometry
-------------------------------------
Getter Method
Signature
MeasuredGeometry()
Returns: Return type: NXOpen.NXObject
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
MeasuredGeometry(face)
Parameters: face ( NXOpen.NXObject
) –New in version NX9.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
NumberOfUPoints¶
-
InspectionUVGridBuilder.
NumberOfUPoints
¶ Returns the number of points in U
-------------------------------------
Getter Method
Signature
NumberOfUPoints()
Returns: Return type: NXOpen.CAM.InheritableIntBuilder
New in version NX7.0.0.
License requirements: None.
NumberOfVPoints¶
-
InspectionUVGridBuilder.
NumberOfVPoints
¶ Returns the number of points in V
-------------------------------------
Getter Method
Signature
NumberOfVPoints()
Returns: Return type: NXOpen.CAM.InheritableIntBuilder
New in version NX7.0.0.
License requirements: None.
NumberOfValidPoints¶
-
InspectionUVGridBuilder.
NumberOfValidPoints
¶ Returns or sets the number of valid points created for the UV Grid
-------------------------------------
Getter Method
Signature
NumberOfValidPoints()
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberOfValidPoints(numPoints)
Parameters: numPoints (int) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PointSequenceDirection¶
-
InspectionUVGridBuilder.
PointSequenceDirection
¶ Returns or sets the point sequence start direction
-------------------------------------
Getter Method
Signature
PointSequenceDirection()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderPointSequenceDirectionTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointSequenceDirection(ptSeqDir)
Parameters: ptSeqDir ( NXOpen.CAM.InspectionMethodBuilderPointSequenceDirectionTypes
) –New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PointSequenceMode¶
-
InspectionUVGridBuilder.
PointSequenceMode
¶ Returns or sets the point sequence mode
-------------------------------------
Getter Method
Signature
PointSequenceMode()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderPointSequenceModeTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointSequenceMode(ptSeqMode)
Parameters: ptSeqMode ( NXOpen.CAM.InspectionMethodBuilderPointSequenceModeTypes
) –New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PointSequenceStart¶
-
InspectionUVGridBuilder.
PointSequenceStart
¶ Returns or sets the point sequence start location
-------------------------------------
Getter Method
Signature
PointSequenceStart()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderPointSequenceStartTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointSequenceStart(ptSeqStart)
Parameters: ptSeqStart ( NXOpen.CAM.InspectionMethodBuilderPointSequenceStartTypes
) –New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RetractDist¶
-
InspectionUVGridBuilder.
RetractDist
¶ Returns the retract distance
-------------------------------------
Getter Method
Signature
RetractDist()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.0.0.
License requirements: None.
SearchDist¶
-
InspectionUVGridBuilder.
SearchDist
¶ Returns the search distance
-------------------------------------
Getter Method
Signature
SearchDist()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.0.0.
License requirements: None.
SequenceOptimization¶
-
InspectionUVGridBuilder.
SequenceOptimization
¶ Returns or sets the path point sequence optimization setting
-------------------------------------
Getter Method
Signature
SequenceOptimization()
Returns: Return type: NXOpen.CAM.InspectionPathBuilderSequenceType
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SequenceOptimization(sequenceOpt)
Parameters: sequenceOpt ( NXOpen.CAM.InspectionPathBuilderSequenceType
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SphereAxisMethod¶
-
InspectionUVGridBuilder.
SphereAxisMethod
¶ Returns or sets the method for determining the axis for a sphere
-------------------------------------
Getter Method
Signature
SphereAxisMethod()
Returns: Return type: NXOpen.CAM.InspectionUVGridBuilderSphereAxisType
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SphereAxisMethod(method)
Parameters: method ( NXOpen.CAM.InspectionUVGridBuilderSphereAxisType
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SphereAxisVector¶
-
InspectionUVGridBuilder.
SphereAxisVector
¶ Returns or sets the sphere axis vector
-------------------------------------
Getter Method
Signature
SphereAxisVector()
Returns: Return type: NXOpen.Direction
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SphereAxisVector(vector)
Parameters: vector ( NXOpen.Direction
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StartPointMode¶
-
InspectionUVGridBuilder.
StartPointMode
¶ Returns or sets the start point mode
-------------------------------------
Getter Method
Signature
StartPointMode()
Returns: Return type: NXOpen.CAM.InspectionUVGridBuilderStartPointType
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartPointMode(startMode)
Parameters: startMode ( NXOpen.CAM.InspectionUVGridBuilderStartPointType
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StartU¶
-
InspectionUVGridBuilder.
StartU
¶ Returns the start value in U
-------------------------------------
Getter Method
Signature
StartU()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.0.0.
License requirements: None.
StartUDeg¶
-
InspectionUVGridBuilder.
StartUDeg
¶ Returns the start degrees value in U
-------------------------------------
Getter Method
Signature
StartUDeg()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: None.
StartUDist¶
-
InspectionUVGridBuilder.
StartUDist
¶ Returns the start distance value in U
-------------------------------------
Getter Method
Signature
StartUDist()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: None.
StartUMode¶
-
InspectionUVGridBuilder.
StartUMode
¶ Returns or sets the start U mode
-------------------------------------
Getter Method
Signature
StartUMode()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderUVModeTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartUMode(uvMode)
Parameters: uvMode ( NXOpen.CAM.InspectionMethodBuilderUVModeTypes
) –New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StartUSweep¶
-
InspectionUVGridBuilder.
StartUSweep
¶ Returns the start sweep value in U
-------------------------------------
Getter Method
Signature
StartUSweep()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: None.
StartV¶
-
InspectionUVGridBuilder.
StartV
¶ Returns the start value in V
-------------------------------------
Getter Method
Signature
StartV()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.0.0.
License requirements: None.
StartVDeg¶
-
InspectionUVGridBuilder.
StartVDeg
¶ Returns the start degrees value in V
-------------------------------------
Getter Method
Signature
StartVDeg()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: None.
StartVDist¶
-
InspectionUVGridBuilder.
StartVDist
¶ Returns the start distance value in V
-------------------------------------
Getter Method
Signature
StartVDist()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: None.
StartVMode¶
-
InspectionUVGridBuilder.
StartVMode
¶ Returns or sets the start V mode
-------------------------------------
Getter Method
Signature
StartVMode()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderUVModeTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartVMode(uvMode)
Parameters: uvMode ( NXOpen.CAM.InspectionMethodBuilderUVModeTypes
) –New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StartVSweep¶
-
InspectionUVGridBuilder.
StartVSweep
¶ Returns the start sweep value in V
-------------------------------------
Getter Method
Signature
StartVSweep()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: None.
Method Detail¶
CopyAttributes¶
-
InspectionUVGridBuilder.
CopyAttributes
¶ Copy point grid parameters
Signature
CopyAttributes(target)
Parameters: target ( NXOpen.CAM.InspectionUVGridBuilder
) –New in version NX9.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SetAppDistChanged¶
-
InspectionUVGridBuilder.
SetAppDistChanged
¶ Flag indicating whether approach distance changed.
Signature
SetAppDistChanged(flag)
Parameters: flag (bool) – New in version NX9.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SetLayoutChanged¶
-
InspectionUVGridBuilder.
SetLayoutChanged
¶ Flag indicating whether layout changed.
Signature
SetLayoutChanged(flag)
Parameters: flag (bool) – New in version NX9.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SetPointCoverageChanged¶
-
InspectionUVGridBuilder.
SetPointCoverageChanged
¶ Flag indicating whether point coverage changed.
Signature
SetPointCoverageChanged(flag)
Parameters: flag (bool) – New in version NX9.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SetPointSequenceChanged¶
-
InspectionUVGridBuilder.
SetPointSequenceChanged
¶ Flag indicating whether point sequence changed.
Signature
SetPointSequenceChanged(flag)
Parameters: flag (bool) – New in version NX9.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SetRetDistChanged¶
-
InspectionUVGridBuilder.
SetRetDistChanged
¶ Flag indicating whether retract distance changed.
Signature
SetRetDistChanged(flag)
Parameters: flag (bool) – New in version NX9.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Validate¶
-
InspectionUVGridBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.