InspectionUVGridBuilderStartPointType Enumeration¶
NXOpen.CAM.InspectionUVGridBuilder.StartPointType is an alias for NXOpen.CAM.InspectionUVGridBuilderStartPointType
-
class
NXOpen.CAM.
InspectionUVGridBuilderStartPointType
¶ Bases:
object
the start point mode
Enum Members
Enum Member Enum Member Description Nearest Nearest pointUminVmin Umin - VminUmaxVmin Umax - VminUminVmax Umin - VmaxUmaxVmax Umax - Vmax-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-