InspectionCparlnFeatureBuilder Class¶
-
class
NXOpen.CAM.
InspectionCparlnFeatureBuilder
¶ Bases:
NXOpen.CAM.OperationBuilder
Represents a CMM Inspection Cparln Feature Builder.
A Cparln is a bounded slot defined by closed ended parallel lines. To create a new instance of this class, use
NXOpen.CAM.InspectionOperationCollection.CreateInspectionCparlnFeatureBuilder()
New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
ChannelName | Returns or sets the channel’s name |
CsysReferenceType | Returns or sets the coordinate system reference type |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndOfPath | Returns the end event builder |
EndType | Returns or sets the end type of the bounded slot or tab (round or square) |
EndUdeSet | Returns the end ude set |
Geometry | Returns the geometry builder |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
InnerOuterType | Returns or sets the inspection feature inner outer type (slot/tab) |
LayoutAndLayer | Returns the Layer and Layout |
Length | Returns or sets the length of the bounded slot or tab |
LengthDirVector | Returns or sets the length direction vector selector |
LengthDirectionI | Returns or sets the slot or tab length direction I component |
LengthDirectionJ | Returns or sets the slot or tab length direction J component |
LengthDirectionK | Returns or sets the slot or tab length direction K component |
LocationPointX | Returns or sets the location point X coordinate at the center of the face of the slot or tab |
LocationPointY | Returns or sets the location point Y coordinate at the center of the face of the slot or tab |
LocationPointZ | Returns or sets the location point Z coordinate at the center of the face of the slot or tab |
MotionOutputBuilder | Returns the motion output builder |
Name | Returns or sets the slot or tab feature name |
NormalDirectionI | Returns or sets the slot or tab normal direction I component |
NormalDirectionJ | Returns or sets the slot or tab normal direction J component |
NormalDirectionK | Returns or sets the slot or tab normal direction K component |
Notes | Returns the notes builder |
OffsetDistance | Returns the offset distance |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
PathDisplayOptions | Returns the path display options builder |
PostToolPathExit | Returns or sets the environment variable that points to the post tool path generation library which has the exit |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
ReverseDirection | Returns or sets the reverse direction button used to reverse the normal direction vector |
SafeClearance | Returns the safe clearance builder |
SelectProjectionFaces | Returns the selector for projection faces |
SelectToolFlag | Returns or sets the user selected tool |
SelectedGeometry | Returns the selected geometry, consisting of two parallel lines |
StartOfPath | Returns the start event builder |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
ToolChangeSetting | Returns the tool change builder |
ToolPathEditor | Returns the Tool Path Editor Builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
Width | Returns or sets the width of the bounded slot or tab |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
FlipNormal | Flips the cparln inspection feature normal vector |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetHoleAxisValues | Get the Hole Axis values @return the Hole Axis values |
GetObject | Returns the object currently being edited by this builder. |
ReverseOffsetDirection | Reverses the offset direction |
SetHoleAxisValues | Set the Hole Axis values |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateEndType | Updates cparln inspection feature characteristic parameters based on selected end type |
UpdateOffset | Updates the cparln inspection feature offset distance and associated values |
UpdateParams | Updates cparln inspection feature characteristic parameters based on selected geometry |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
InspectionCparlnFeatureBuilderEndTypes Enumeration | The shape of the end of the bounded slot/tab (round or square) |
Property Detail¶
CsysReferenceType¶
-
InspectionCparlnFeatureBuilder.
CsysReferenceType
¶ Returns or sets the coordinate system reference type
-------------------------------------
Getter Method
Signature
CsysReferenceType()
Returns: Return type: NXOpen.CAM.CamInspectionOperationCsysreferencetypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CsysReferenceType(csysReferenceType)
Parameters: csysReferenceType ( NXOpen.CAM.CamInspectionOperationCsysreferencetypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EndType¶
-
InspectionCparlnFeatureBuilder.
EndType
¶ Returns or sets the end type of the bounded slot or tab (round or square)
-------------------------------------
Getter Method
Signature
EndType()
Returns: Return type: NXOpen.CAM.InspectionCparlnFeatureBuilderEndTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndType(endType)
Parameters: endType ( NXOpen.CAM.InspectionCparlnFeatureBuilderEndTypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
InnerOuterType¶
-
InspectionCparlnFeatureBuilder.
InnerOuterType
¶ Returns or sets the inspection feature inner outer type (slot/tab)
-------------------------------------
Getter Method
Signature
InnerOuterType()
Returns: Return type: NXOpen.CAM.CamInspectionOperationInneroutertypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InnerOuterType(innerOuterType)
Parameters: innerOuterType ( NXOpen.CAM.CamInspectionOperationInneroutertypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Length¶
-
InspectionCparlnFeatureBuilder.
Length
¶ Returns or sets the length of the bounded slot or tab
-------------------------------------
Getter Method
Signature
Length()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Length(length)
Parameters: length (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LengthDirVector¶
-
InspectionCparlnFeatureBuilder.
LengthDirVector
¶ Returns or sets the length direction vector selector
-------------------------------------
Getter Method
Signature
LengthDirVector()
Returns: Return type: NXOpen.Direction
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LengthDirVector(lengthDirVector)
Parameters: lengthDirVector ( NXOpen.Direction
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LengthDirectionI¶
-
InspectionCparlnFeatureBuilder.
LengthDirectionI
¶ Returns or sets the slot or tab length direction I component
-------------------------------------
Getter Method
Signature
LengthDirectionI()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LengthDirectionI(lengthDirectionI)
Parameters: lengthDirectionI (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LengthDirectionJ¶
-
InspectionCparlnFeatureBuilder.
LengthDirectionJ
¶ Returns or sets the slot or tab length direction J component
-------------------------------------
Getter Method
Signature
LengthDirectionJ()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LengthDirectionJ(lengthDirectionJ)
Parameters: lengthDirectionJ (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LengthDirectionK¶
-
InspectionCparlnFeatureBuilder.
LengthDirectionK
¶ Returns or sets the slot or tab length direction K component
-------------------------------------
Getter Method
Signature
LengthDirectionK()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LengthDirectionK(lengthDirectionK)
Parameters: lengthDirectionK (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LocationPointX¶
-
InspectionCparlnFeatureBuilder.
LocationPointX
¶ Returns or sets the location point X coordinate at the center of the face of the slot or tab
-------------------------------------
Getter Method
Signature
LocationPointX()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LocationPointX(locationPointX)
Parameters: locationPointX (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LocationPointY¶
-
InspectionCparlnFeatureBuilder.
LocationPointY
¶ Returns or sets the location point Y coordinate at the center of the face of the slot or tab
-------------------------------------
Getter Method
Signature
LocationPointY()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LocationPointY(locationPointY)
Parameters: locationPointY (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LocationPointZ¶
-
InspectionCparlnFeatureBuilder.
LocationPointZ
¶ Returns or sets the location point Z coordinate at the center of the face of the slot or tab
-------------------------------------
Getter Method
Signature
LocationPointZ()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LocationPointZ(locationPointZ)
Parameters: locationPointZ (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Name¶
-
InspectionCparlnFeatureBuilder.
Name
¶ Returns or sets the slot or tab feature name
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
NormalDirectionI¶
-
InspectionCparlnFeatureBuilder.
NormalDirectionI
¶ Returns or sets the slot or tab normal direction I component
-------------------------------------
Getter Method
Signature
NormalDirectionI()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalDirectionI(normalDirectionI)
Parameters: normalDirectionI (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
NormalDirectionJ¶
-
InspectionCparlnFeatureBuilder.
NormalDirectionJ
¶ Returns or sets the slot or tab normal direction J component
-------------------------------------
Getter Method
Signature
NormalDirectionJ()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalDirectionJ(normalDirectionJ)
Parameters: normalDirectionJ (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
NormalDirectionK¶
-
InspectionCparlnFeatureBuilder.
NormalDirectionK
¶ Returns or sets the slot or tab normal direction K component
-------------------------------------
Getter Method
Signature
NormalDirectionK()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalDirectionK(normalDirectionK)
Parameters: normalDirectionK (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
OffsetDistance¶
-
InspectionCparlnFeatureBuilder.
OffsetDistance
¶ Returns the offset distance
-------------------------------------
Getter Method
Signature
OffsetDistance()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.0.
License requirements: None.
ReverseDirection¶
-
InspectionCparlnFeatureBuilder.
ReverseDirection
¶ Returns or sets the reverse direction button used to reverse the normal direction vector
-------------------------------------
Getter Method
Signature
ReverseDirection()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseDirection(reverseDirection)
Parameters: reverseDirection (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SelectProjectionFaces¶
-
InspectionCparlnFeatureBuilder.
SelectProjectionFaces
¶ Returns the selector for projection faces
-------------------------------------
Getter Method
Signature
SelectProjectionFaces()
Returns: Return type: NXOpen.SelectFace
New in version NX7.0.0.
License requirements: None.
SelectedGeometry¶
-
InspectionCparlnFeatureBuilder.
SelectedGeometry
¶ Returns the selected geometry, consisting of two parallel lines
-------------------------------------
Getter Method
Signature
SelectedGeometry()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX7.0.0.
License requirements: None.
Width¶
-
InspectionCparlnFeatureBuilder.
Width
¶ Returns or sets the width of the bounded slot or tab
-------------------------------------
Getter Method
Signature
Width()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Width(width)
Parameters: width (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
FlipNormal¶
-
InspectionCparlnFeatureBuilder.
FlipNormal
¶ Flips the cparln inspection feature normal vector
Signature
FlipNormal()
New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ReverseOffsetDirection¶
-
InspectionCparlnFeatureBuilder.
ReverseOffsetDirection
¶ Reverses the offset direction
Signature
ReverseOffsetDirection()
New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UpdateEndType¶
-
InspectionCparlnFeatureBuilder.
UpdateEndType
¶ Updates cparln inspection feature characteristic parameters based on selected end type
Signature
UpdateEndType()
New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UpdateOffset¶
-
InspectionCparlnFeatureBuilder.
UpdateOffset
¶ Updates the cparln inspection feature offset distance and associated values
Signature
UpdateOffset()
New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UpdateParams¶
-
InspectionCparlnFeatureBuilder.
UpdateParams
¶ Updates cparln inspection feature characteristic parameters based on selected geometry
Signature
UpdateParams()
New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Validate¶
-
InspectionCparlnFeatureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.