InspectionCparlnFeatureBuilderEndTypes Enumeration

NXOpen.CAM.InspectionCparlnFeatureBuilder.EndTypes is an alias for NXOpen.CAM.InspectionCparlnFeatureBuilderEndTypes

class NXOpen.CAM.InspectionCparlnFeatureBuilderEndTypes

Bases: object

The shape of the end of the bounded slot/tab (round or square)

Enum Members

Enum Member Enum Member Description
Round
Bounded slot/tab has round end
Square
Bounded slot/tab has square end
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.