CamInspectionOperationCsysreferencetypes Enumeration

class NXOpen.CAM.CamInspectionOperationCsysreferencetypes

Bases: object

Coordinate system that the inspection feature data is relative to Enum Members

Enum Member Enum Member Description
RelativetoPCS
Relative to Part Coordinate System
Absolute
Relative to Absolute Coordinate System
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.