AlignmentType |
Returns or sets the alignment type |
ChannelName |
Returns or sets the channel’s name |
CycleEvent |
Returns the cycle event |
CycleTable |
Returns the cycle |
Description |
Returns or sets the description |
EndOfPath |
Returns the end event builder |
EndUdeSet |
Returns the end ude set |
Geometry |
Returns the geometry builder |
GougeChecking |
Returns or sets the gouge checking flag |
HoleAxisType |
Returns or sets the Hole Axis Type |
HoleDepth |
Returns the max depth distance builder |
HoleDepthType |
Returns or sets the Hole Depth Type |
IterativeMax |
Returns or sets the maximum number of iterations |
IterativeRotation |
Returns or sets the iterative rotation convergence value |
IterativeToggle |
Returns or sets the iterative toggle |
IterativeTranslation |
Returns or sets the iterative translation convergence value |
IterativeType |
Returns or sets the iterative type |
LayoutAndLayer |
Returns the Layer and Layout |
MotionOutputBuilder |
Returns the motion output builder |
Notes |
Returns the notes builder |
OperationName |
Returns or sets the operation name |
OptimizationBasedOn |
Returns or sets the optimization based on in operation |
OptimizationDistanceMethod |
Returns or sets the optimization distance method in operation |
OptimizationLevel |
Returns or sets the optimization level in operation |
OptimizationMethod |
Returns or sets the optim method |
PathDisplayOptions |
Returns the path display options builder |
PostToolPathExit |
Returns or sets the environment variable that points to the post tool path generation library which has the exit |
PrimaryDirection |
Returns or sets the primary direction |
PrimaryOffsetGeometry |
Returns or sets the primary offset geometry |
PrimarySelection |
Returns the primary selection |
PrimaryState |
Returns or sets the primary state |
PrimaryType |
Returns or sets the primary feature type |
RetractDistance |
Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange |
Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
SafeClearance |
Returns the safe clearance builder |
SecondaryDirection |
Returns or sets the secondary direction |
SecondaryOffsetGeometry |
Returns or sets the secondary offset geometry |
SecondarySelection |
Returns the secondary selection |
SecondaryState |
Returns or sets the secondary state |
SecondaryType |
Returns or sets the secondary feature type |
SelectToolFlag |
Returns or sets the user selected tool |
StartOfPath |
Returns the start event builder |
StartUdeSet |
Returns the start ude set |
Tag |
Returns the Tag for this object. |
TertiaryDirection |
Returns or sets the tertiary direction |
TertiaryOffsetGeometry |
Returns or sets the tertiary offset geometry |
TertiarySelection |
Returns the tertiary selection |
TertiaryState |
Returns or sets the tertiary state |
TertiaryType |
Returns or sets the tertiary feature type |
ToolChangeSetting |
Returns the tool change builder |
ToolPathEditor |
Returns the Tool Path Editor Builder |
ToolPathSplitParametersBuilder |
Returns the tool path split Parameters |