InspectionAlignmentAssistantBuilderFeatureType Enumeration¶
NXOpen.CAM.InspectionAlignmentAssistantBuilder.FeatureType is an alias for NXOpen.CAM.InspectionAlignmentAssistantBuilderFeatureType
-
class
NXOpen.CAM.
InspectionAlignmentAssistantBuilderFeatureType
¶ Bases:
object
Alignment feature type
Enum Members
Enum Member Enum Member Description Plane Plane alignment feature typeBestFitPlane Best Fit Plane alignment feature typeOffsetPlane Offset Plane alignment feature typeMidPlane Mid Plane alignment feature typeCylinder Cylinder alignment feature typeBestFitCylinder Best Fit Cylinder alignment feature typeLine Line alignment feature typeBestFitLine Best Fit Line alignment feature typeIntersectLine Intersect Line alignment feature typeCircle Circle alignment feature typeBestFitCircle Best Fit Circle alignment feature typePoint Point alignment feature typeBestFitPoint Best Fot Point alignment feature type-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-